Hi there )))I have the TP177micro panel 6AV6 640-0CA11-0AX1. The display isnt working normally, it doesnt show 90% of information. There`s a blue screen on it, but at the middle of a screen threre`s a band, part of screen that working normally (the photo`s are attached). So i think, that the HW and touchscreen of a panel is working great, the display is broken, cause when starting the panel, i can see the booting process, startup menu and mnemo in that 10 working percents of a screen. So. I want to backup the project from panel by WinCC 2008 Flex SP3. When i choose the backup command in wincc, i restart the panel, and then there is an error message, that saying to set the transfer mode in panel. Of course, i can`t, because i don`t see anything. I want to try do the backup BLINDLY. So, if anybody have same panel, can you send me video or pics with the instruction, where on screen i have to tap, step by step, to set the transfer mode on panel, and do the backup.
It`s more likely that recreate the existing project

Thank you for your help.
=== Edited by Dan_Tien_Shan @ 8/6/2012 1:09 PM [GMT ] ===
|