Technical Forum

LOGO!

Logo 6 <> logo 7

Thread Starter: Paulvdbo   Started: 8/2/2012 7:33 AM   Replies: 5

« Previous thread Next thread »
Page 1 of 1 (6 items)
  8/2/2012, 7:33 AM
Joined 12/20/2011
Last visit: 6/17/2013
Posts: 24
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear friends,
Can anyone tell me why I only can use a Logo 7 for this project ? I don't need any of the special/new Logo 7 features ...

*** Determine LOGO!
Resources used:
Function Blocks         40/400
REM                     0/250
Digital Inputs          4/24
Digital Outputs         4/16
Flag                    2/27
Analog Inputs           0/8
Text Box                6/50
Text contents           6/50
Analog outputs          0/2
Program memory          580/8000
Block names             0/100
Analog flags            1/16
Cursor keys             0/4
Shift register          0/4
Shift register bits     0/32
Open connectors         0/64
LOGO! TD Function keys  0/4
Network inputs          0/64
Network analog inputs   0/32
UDF types               0/16
UDF instances           0/64
Data Log                0/1
Network outputs         0/64
Network analog outputs  0/16
Analog Filters          0/8
Maximum nesting depth: I1-B008-B037-B006-B010-B023-B004-B041-Q1

The following LOGO! can be used:
0BA7.Standard

Thanks in advace ! laugh
Top
  8/2/2012, 8:10 AM
Joined 7/24/2006
Last visit: 6/19/2013
Posts: 1843
Rating:
Rated: Outstanding [3.68 out of 5 / rated 217 time(s)]. (217) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

You have used at least on feature not supported in older LOGO!

Post your program to see what it is.

Regards
Top
Thank you for this post from:
  8/2/2012, 10:41 AM
Joined 12/20/2011
Last visit: 6/17/2013
Posts: 24
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanks for your concern, Helmut.
I add the diagram. Nevertheless it's weird 'cause I MADE the prog in 6, but after I opened it in 7, it only worked with 7 afterwards....

btw... it's not completely finished yet ...

Attachment: test pomp.zip  (20 Downloads)



=== Edited by Paulvdbo @ 8/2/2012 10:42 AM [GMT ] ===



Top
  8/2/2012, 12:49 PM
Joined 12/27/2006
Last visit: 6/19/2013
Posts: 419
Rating:
Rated: Excellent [4.24 out of 5 / rated 21 time(s)]. (21) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
If you change the TEXT blocks , then you canb use alse the 0BA5 or 0BA6.
Try this at home:
F2 (= TOOLS > Determineer LOGO)  Look in the Info screen.
Scroll upside.
her you can find with LOGO you can use, but als look why an older LOGO dont fit.

You can als see whats wrong in your programm. You cant send it from your PC to the logo, because several blockt ( the textblocks) have no connection on the output.
In the LOGO! every block MUST have an output connection.
You can yse the " Open Connector" Block .

Next time start an new programm an as first you chose the richt LOGO! with CTRL+H (TOOLS > Select Hardware) Then you cant make a programm thats not fix in your LOGO!
Top
Thank you for this post from:
  8/2/2012, 1:16 PM
Joined 12/20/2011
Last visit: 6/17/2013
Posts: 24
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thank you toeternitoe,

I know that the program won't be transferable to "any" logo YET. But that was not my main question.
Even removal of the text blocks still doesn't allow me to "use" a OBA6 ...
Here's the info of the same program, but with all Text blocks removed :
*** Determine LOGO!
Resources used:
Function Blocks         30/400
REM                     0/250
Digital Inputs          4/24
Digital Outputs         4/16
Flag                    2/27
Analog Inputs           0/8
Text Box                0/50
Text contents           0/50
Analog outputs          0/2
Program memory          460/8000
Block names             0/100
Analog flags            1/16
Cursor keys             0/4
Shift register          0/4
Shift register bits     0/32
Open connectors         0/64
LOGO! TD Function keys  0/4
Network inputs          0/64
Network analog inputs   0/32
UDF types               0/16
UDF instances           0/64
Data Log                0/1
Network outputs         0/64
Network analog outputs  0/16
Analog Filters          0/8
Maximum nesting depth: I1-B008-B037-B006-B010-B023-B004-B041-Q1

The following LOGO! can be used:
0BA7.Standard
Top
  8/2/2012, 1:22 PM
Joined 12/20/2011
Last visit: 6/17/2013
Posts: 24
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Aha ! OK ... the [Select Hardware] indeed showed me what blocks are not possible in OAB6 !
I'll find a work-around for those things.

Thanks Toeternitoe !
Top
Page 1 of 1 (6 items)
Actions