Technical Forum

SIMATIC WinCC

install wincc server 6.2

Thread Starter: A.control   Started: 7/31/2012 8:23 AM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  7/31/2012, 8:23 AM
Joined 6/30/2011
Last visit: 9/19/2012
Posts: 88
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear all,

I  must install wincc server 6.2, I have the license of server but not the cd of that, but i have the wincc 6.2 RC which is used by engineering station.

So i used the same cd but only installed RT  option of it on my server, and then transfered the server license to  it.  now i have some problems  and i want to make sure  is this kind of installation can cause a problem or I must look for the cause in somewhere else?

So in another word:  can I  install wincc server from an wincc cd for engineering station which containes both RC and RT, and deselect the RC option when installing?

Best Regards



=== Edited by O_Moderator @ 7/31/2012 10:11 PM [GMT ] ===
new subject after splitting from Do I need to install connectivity pack V6.1 SP1 server on the server?

Top
  8/1/2012, 2:07 AM
Joined 1/10/2008
Last visit: 5/10/2013
Posts: 2485
Rating:
Rated: Outstanding [3.77 out of 5 / rated 209 time(s)]. (209) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
A.control wrote:
. . . in another word:  can I  install wincc server from an wincc cd for engineering station which containes both RC and RT, and deselect the RC option when installing?
Yes.
Top
Thank you for this post from:
  8/1/2012, 9:55 AM
Joined 10/5/2010
Last visit: 5/22/2013
Posts: 1355
Rating:
Rated: Outstanding [3.79 out of 5 / rated 34 time(s)]. (34) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello A.control,

I agree with Phantom75.

So what problems do you have after installation?

Please let me know, whether I can help you.

Best regards

Bizur
Top
Thank you for this post from:
  8/4/2012, 7:41 AM
Joined 6/30/2011
Last visit: 9/19/2012
Posts: 88
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Bizur wrote:
Hello A.control,
So what problems do you have after installation?

Please let me know, whether I can help you.



 Dear Bizur,

Thank you very much.

Well the problem is:  when  I install wincc RT on server and transfer project from engineering laptop to the server, the project is ported compeletly, but the icon of *.mcp  file is not like the wincc icon it is apprears like an unknown file format.

I thought maybe after a restart it is shown correctly, so I set the project in autostart and then restarted the server computer, but it didn't apear correctly.

I had no other way, I installed wincc compeletly, it means now I have both RC and RT on server, now the project comes up correctly and the icon of  *.mcp  file is  look like wincc.

As you know, normally there musn't be  any configuration option on server, besides I don't have any extra RC license to permenantly transfer to server. In other words I cannot go on working with RC installed on my server, I have to understand the problem and Uninstall the RC from server.

Any help or idea is appreciated in advance

Best Regards
Top
  8/10/2012, 11:06 AM
Joined 10/5/2010
Last visit: 5/22/2013
Posts: 1355
Rating:
Rated: Outstanding [3.79 out of 5 / rated 34 time(s)]. (34) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello A.control,

this is really a strange behaviour.
Do you have just this one station?
Does it happen to all your projects?

Please let me know

Bizur
Top
Page 1 of 1 (5 items)
Actions