Technical Forum

SIMODRIVE Converter system

SimoDrive Terminals

Thread Starter: Karnan   Started: 7/30/2012 7:35 AM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  7/30/2012, 7:35 AM
Joined 12/16/2011
Last visit: 5/17/2013
Posts: 217
Rating:
Rated: Outstanding [4 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hai All,

Please Anyone clear my doubt about Terminals of SimoDrive,

What is the function of "Reset"[pin 15,R] ??

What are the condition to activate internal "Start Inhibit" relay[AS1,AS2] is it ralates to " Setup operation"[112]??

Thanks&Regards,
Raj

Top
  9/5/2012, 1:18 PM
Joined 6/15/2012
Last visit: 4/25/2013
Posts: 5
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Karman Hello, I think I can help you.
The terminal 15 / R connector x141 serves to reset the fault (for example, lack of phase) of the unit.
The terminal X172 (AS1 and AS2) are NC contacts are open when you enable 112/9 (Operation).


Top
Thank you for this post from:
Page 1 of 1 (2 items)
Actions