Technical Forum

Decentral Peripherie

IM-module troubles

Thread Starter: S7-FreshMan   Started: 7/29/2012 8:58 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  7/29/2012, 8:58 PM
Joined 11/14/2008
Last visit: 5/13/2013
Posts: 185
Rating:
Rated: Excellent [4.67 out of 5 / rated 3 time(s)]. (3) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi ,
I've got next problem with IM 151-3 (6ES7151-3BA23-0AB0) :
I'm using version 7.0 of this module in HW Config in Simatic manager.
After adding this IM-module to an ethernet-network, I have tried to add some I/O and F-I/O to this module (within the powermodules). I have noticed that their exists different versions ( of this IM-module. in some of the versions of the IM-module it is possible to find back an F-I/O card , although it is not possible to find an F-I/O module in the system family of IM 151-3 version 7.0.
When I do a search after the F-module that I want to add , Simatic manager finds the card back in an older version of the IM 151-3 (e.g. v4.0) , but when I try to add this module in the rack of IM 151-3 version 7.0 , he says that it is not the same system family.
I have installed all latest updates of simatic manager and distributed safety and also F-configuration pack.
My question for you is , how can I make a configuration with standard I/O and F-I/O within one IM 151-3 ?
Because when I take IM 151-3 v4.0 where the F-I/O does exists than the problem is that he won't find the standard modules in this system family 4.0 ..
Thanks in advance,
Hereby I'm also sending my configuration in attachments.


Attachment: Hw_Config.jpg  (7 Downloads)

Top
  7/30/2012, 8:58 PM
Joined 11/14/2008
Last visit: 5/13/2013
Posts: 185
Rating:
Rated: Excellent [4.67 out of 5 / rated 3 time(s)]. (3) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Problem solved with installation of F-Configuration Pack V5.5 + SP9+ Upd 1.
Top
Thank you for this post from:
Page 1 of 1 (2 items)
Actions