Technical Forum

Process Instrumentation / Analytics / Weighing Systems SIWAREX

Simatic PDM Device Management Problem

Thread Starter: ozkececi   Started: 7/25/2012 2:50 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  7/25/2012, 2:50 PM
Joined 5/2/2012
Last visit: 8/24/2012
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

I have some problems with Simatic PDM.When I try to select devices from device catalog,it gives 2 error;

--------------------------------------------------------------------------------------------------

1)  DL compiler error : c:\program
files\siemens\pdm\sim_pdm\devices\si__dev01.cfg(943)

2)  Device description could not be loaded.
Please install it in the SIMATIC Manager using
'SIMATIC PDM Manage Device Catalog' or reinstall
SIMATIC PDM.

------------------------------------------------------------------------------------------------

* I installed device catalog again and then installed all of the devices.
* And I also reinstalled Simatic PDM.

This problem doesnt let me to choose device.

Also I attached an image about the problem...

My Simatic Manager: V5.5,SP1
Simatic PDM:V6.0,SP3

Does anyone has any idea about this problem ?Rnf:lblSmileyTooltip_

Thanks in advance,

Attachment: PDM problem.JPG  (15 Downloads)

Top
  7/26/2012, 5:46 AM
Joined 6/13/2006
Last visit: 4/15/2013
Posts: 186
Rating:
Rated: Excellent [4.83 out of 5 / rated 6 time(s)]. (6) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

I had the same problem before but after I reinstall the devices library CD, the probles can be solved.

Perhaps you need to install the devices library CD V6_SP_5 and make sure you sellect all options are required for PDM (Do not only select " Siemens " )


 Regards
chook



=== Edited by Chook @ 7/26/2012 5:51 AM [GMT ] ===




Top
Page 1 of 1 (2 items)
Actions