Technical Forum

LOGO!

OBA7 multiple units on network

Thread Starter: Thermal1   Started: 7/24/2012 3:10 AM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  7/24/2012, 3:10 AM
Joined 7/24/2012
Last visit: 7/24/2012
Posts: 0
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hi, I have 2x OBA7 running as master slave, and is operating well.
How do I network multiple units plus monitor remotely via PC, I expect an ethernet switch or hub is required??
This will also hopefully allow online monitoring as currently I have to disconnect the slave unit and connect the PC which drops out half of my I/O.

Assistance greatly appreciated.

Top
  7/24/2012, 11:52 AM
Joined 7/24/2006
Last visit: 5/16/2013
Posts: 1823
Rating:
Rated: Outstanding [3.68 out of 5 / rated 216 time(s)]. (216) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

you are right, you need a switch.

Goto: www.siemens.com/logo.

Siemens offers two switches in LOGO! Design called CSM (24V & 230V versions).

Hope this helps
Top
Thank you for this post from:
Page 1 of 1 (2 items)
Actions