Technical Forum

SIMATIC WinCC flexible

Error when install wincc flexible 2008 in XP Mode

Thread Starter: Avtomatvs   Started: 7/23/2012 10:14 PM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  7/23/2012, 10:14 PM
Joined 6/26/2012
Last visit: 2/13/2013
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

I've got VM XpMode to run 32bits softwares, since my machine run in Win7 64 bits, so I try install Wincc Flexible 2008 in the Xp mode and this errors occur(see attachment):

WinCC flexible Error
Error 1722. There is a problem with this Windows Installer package. A program run as part of the setup did not finish as expected. Contact your support personnel or package vendor. Action _F4F465C5_0854_4B21_92CB_8CBCC15B626E, location: C:\WINDOWS\system32\OpcEnum.exe, command: /RegServer

The following mesage appears:

Feature transfer error
Consult Windows Installer Help(Msi.chm) or MSDN for more information.

And the setup finishes without installing.

How I fix it?

Attachment: error install winccflex 2008.jpg  (27 Downloads)

Top
  7/24/2012, 12:25 AM
Joined 5/28/2008
Last visit: 5/22/2013
Posts: 2187
Rating:
Rated: Outstanding [3.65 out of 5 / rated 431 time(s)]. (431) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Avtomatvs wrote:
Hi,

I've got VM XpMode to run 32bits softwares, since my machine run in Win7 64 bits, so I try install Wincc Flexible 2008 in the Xp mode and this errors occur(see attachment):

WinCC flexible Error
Error 1722. There is a problem with this Windows Installer package. A program run as part of the setup did not finish as expected. Contact your support personnel or package vendor. Action _F4F465C5_0854_4B21_92CB_8CBCC15B626E, location: C:\WINDOWS\system32\OpcEnum.exe, command: /RegServer

The following mesage appears:

Feature transfer error
Consult Windows Installer Help(Msi.chm) or MSDN for more information.

And the setup finishes without installing.

How I fix it?
Hello,
Please check the compatability between your OS installed on VM & WinCC flexible using this FAQ:
Hope this helps.

Ayman Elotaify
MISC Egypt
www.miscegypt.com
Top
  7/24/2012, 4:36 PM
Joined 6/26/2012
Last visit: 2/13/2013
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
According to the microsoft site "Windows XP Mode installs a virtual hard disk file that contains Windows XP Professional Service Pack 3", and the Compatibility Tool resulted in compatible (this I knew, because I had already installed WinCC flexible 2008 in Win XP Professional SP3) but still the error occur in XP Mode.

Another question:
If I install WinCC flexible SP3 in Windows7 64bits, create a project and then opening the project created in WinCC flexible SP3(or even SP2) in Win XP 32bits, does it work?
Top
  7/25/2012, 11:50 AM
Joined 9/5/2011
Last visit: 5/23/2013
Posts: 2587
Rating:
Rated: Outstanding [3.83 out of 5 / rated 132 time(s)]. (132) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

You should use the Cleanup Support Tool at this behaviour.
See the following link.

What can cause the installation to abort or prevent successful starting of WinCC flexible?

You can open a project of WinCC flexible 2008 SP2 with WinCC flexible 2008 SP3.
You can not open a project of WinCC flexible 2008 SP3 with WinCC flexible 2008 SP2.
That is not possible.


Tweety
Top
Thank you for this post from:
Page 1 of 1 (4 items)
Actions