Hi All,
My client is having a S7 200 CPU 224 CN with 3 number of EM modules and the configuration is shown below,
| CPU 224 -CN | 214-1AD23-0XB8 | DC/DC/DC |
| EM 231 CN | 231-1HC22-0XA8 | AI4 X 12 Bit |
| EM 222 CN | 222-1BF22-0XA8 | DO 1 Byte |
| EM 232 CN | 232-0HB22-0XA8 | AO - 2 Channel X 12 Bit |
The CPU 224 CN is failed, so they want to replace it with another CPU which is not (CN) Chinese graded.
| CPU 224 | 214-1AD23-0XB0 | DC/DC/DC
|
Is it possible to use the CN grade extension modules with the normal CPU 224.
Microwin is not having hardware configuration to check the compatability of such situation.
_______________________________________________________________
Best Regards
T.Saravana Kumar
"All for the Best"