Technical Forum

Meet & Talk

Dynamic value in FM458 function diagram is disappear

Thread Starter: Norm47   Started: 7/18/2012 12:36 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  7/18/2012, 12:36 PM
Joined 7/18/2012
Last visit: 7/20/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello

The dynamic value in FM458 function diagram is disappear after long time operation of SPPA-T3000.I checked signal in ProfiSignal software still archived to file. But the trouble happen when I want to analyse the Gas Turbine control functions, because no any dynamic values were show.
I don't want to reboot the ftServer, right now. It may be the last choice.

Has anyone can help? sad

Thanks

Norm47

Attachment: 51_52FM458_NotShow_001.JPG  (5 Downloads)

Top
  7/20/2012, 1:48 AM
Joined 7/18/2012
Last visit: 7/20/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Can do I stop and restart a special file in Application server from Windows service or Task manager
I never do sure to touch the Application server during plant operation, the operator will not happy
when the dynamic value monitoring on their graphic display are interrupted.

cry
Top
Page 1 of 1 (2 items)
Actions