Technical Forum

SIMATIC WinCC flexible

wincc flexible 2008 sp3 project creation problem

Thread Starter: newyguy   Started: 7/14/2012 10:53 AM   Replies: 6

« Previous thread Next thread »
Page 1 of 1 (7 items)
  7/14/2012, 10:53 AM
Joined 7/14/2012
Last visit: 8/15/2012
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I installed wincc flexible 2008 sp3 on windows 7 x64 completely with no problem

after I started wincc, it asked me to create an empty project first.

when I clicked "create an empty project", it loaded a few things and
then this error message showed up:

"creation of the template failed.Try to create the project again.
If it fails agian, contact support.
A file with this name already exist."

Note: I had installed Step 7 v5.5 SP2 before installing wincc.

So what did I do wrong? and what should I do??

Attachment: error.jpg  (32 Downloads)

Top
  7/16/2012, 1:11 PM
Joined 7/14/2012
Last visit: 8/15/2012
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I found this post which dates back to 4 years ago. someone with the same problem as me
and nobody answered him

https://support.automation.siemens.com/WW/llisapi.dll?query=Creation+of+the+template&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx%3Ftab%3D2&lang=en&siteid=csius&objaction=cssearch&searchinprim=_searchinprim_&nodeid=99&x=16&y=8&cssearchengine=NEW&x=18&y=9

I'm beginig to think no one knows how to fix this problem...
Top
  7/16/2012, 4:57 PM
Joined 9/5/2011
Last visit: 5/17/2013
Posts: 2549
Rating:
Rated: Outstanding [3.83 out of 5 / rated 131 time(s)]. (131) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello newyguy,

You should do the point 2.1 in the following FAQ.

What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted?

Tweety
Top
  7/16/2012, 6:20 PM
Joined 7/14/2012
Last visit: 8/15/2012
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 


thanks for the tip but I've already read through all that page and did all
the points necessary including 2.1 but still no luck.

I'll keep trying to fix it and I appreciate it if anyone else have other solutions
to share.

I think the last option would be to re-install the whole windows 7.
Top
  7/17/2012, 3:26 PM
Joined 9/5/2011
Last visit: 5/17/2013
Posts: 2549
Rating:
Rated: Outstanding [3.83 out of 5 / rated 131 time(s)]. (131) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

You should check the list on the end of the following FAQ:

With what are SIMATIC WinCC flexible 2008, 2007, 2005 and 2004 compatible?


Do you do a repair instalation of WinCC flexible?

Tweety
Top
  7/18/2012, 4:59 PM
Joined 7/14/2012
Last visit: 8/15/2012
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Tweety wrote:
Hello,

You should check the list on the end of the following FAQ:

With what are SIMATIC WinCC flexible 2008, 2007, 2005 and 2004 compatible?


Do you do a repair instalation of WinCC flexible?

Tweety


my wincc flexible is 2008 sp3 which is compatible with 7 x64

I installed it once. then completely removed it with all the SQL programs I had (all of them)
from add and remove.

then installed wincc again.

should I repair it?



=== Edited by newyguy @ 7/18/2012 5:00 PM [GMT ] ===


Top
  7/19/2012, 11:02 AM
Joined 9/5/2011
Last visit: 5/17/2013
Posts: 2549
Rating:
Rated: Outstanding [3.83 out of 5 / rated 131 time(s)]. (131) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello

Yes, you should use the repair installation of WinCC flexible.

Tweety
Top
Page 1 of 1 (7 items)
Actions