Technical Forum

DC converters SIMOREG

6RA80 auto current controller optimisation

Thread Starter: DK.   Started: 7/9/2012 8:07 AM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  7/9/2012, 8:07 AM
Joined 12/28/2007
Last visit: 3/16/2013
Posts: 20
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
  Dear All,

I am using below drive and when I tries to optimise armature current controller in auto (P50051=25) actual armature current goes up to 240% of rated motor current (p50100).

Drive Number - 6RA8025-6DS22-0AA0-Z
Drive rating - 60A & 415V
P076 = 70% = 41.92 Amp
P50100 = 38A

During P50051=25 armature actual current went up to 92Amp. (r50117 = 220% = 92Amp )
(r50019 = 240% = 92Amp)

Kindly let me know why such things should happened because as per manual during current controller optimisation in auto armature current will rise up to 75% of motor rated current.

In 6RA70 I never face such problem.

Thanks & Regards, 

DK
Top
  7/10/2012, 7:05 AM
Joined 4/23/2010
Last visit: 5/23/2013
Posts: 1148
Rating:
Rated: Outstanding [3.17 out of 5 / rated 53 time(s)]. (53) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,
Before starting otimisation, have you adjust the rated unit currents? Please check the attached sheet.

Attachment: 6RA80 commissioning.pdf  (32 Downloads)

Tell me and I will forget. Show me and I will remember. Involve me and I will understand. -Confucius

Top
  7/14/2012, 5:39 AM
Joined 12/28/2007
Last visit: 3/16/2013
Posts: 20
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hello...

everything was setted well... afetr auto optimisation I did the manual optimsation of current controller and step responces OK howevevr again I tried to do auto optimisation then actual current goes upto 220%. Generally it must go up 70% and some peaks (spikes) can go up to 120% as my experince in 6RA70.

Kindly do the needful.

Thnks & regards,

DK
Top
Page 1 of 1 (3 items)
Actions