SIMOVERT MASTERDRIVES
Profibus speed parameters CUVC
Thread Starter: candy Started: 7/13/2012 11:07 PM Replies: 0

7/13/2012, 11:07 PM
|
Joined 7/13/2012
Last visit: 7/13/2012
Posts: 1
Rating:
(0)
|
(0)
|
the Problem: We have machines with siemens maser drivers with differed profibus speeds some are 500 some run on 1,5 now on the shelf we got like 20 CUVC cards some times when we replace a card ( yes we do the full Monty P60 change settings enter profibus-address and motor type then factory reset put P60 back ect ect ) after that the card is ready to get its parameters but some times , the card and the S7 CPU give a profibus error because there running on a different speeds. Its always a gamble if you have the correct one. If it is set to a wrong speed, i have to : 1. shoot the parameters in via de serial bus means i have to take the Field PG with me every time. its not always easy access place, or up to date ....
2. or change the speed of the profibus in the project and shoot it over via ether net to the S7CPU . so i can use drive monitor via the profibus. after the drive gets the new parameters i have to change the speed of the profibus back to original settings. its a work around.
my question I'm / we are having trouble with finding the profibus speed parameter in the CUVC manual. or is there a way to change/check the settings manually? if so what P/R address do i change / check?
mvg mike
=== Edited by candy @ 7/13/2012 11:10 PM [GMT ] ===
|
|
|
|
|
Actions