Technical Forum

Process Control Systems SIMATIC PCS 7

Project Error after PCS7 V7.1 Upgrade to Sp1

Thread Starter: Navnag   Started: 8/27/2010 7:16 PM   Replies: 13

« Previous thread Next thread »
12» Page 1 of 2 (14 items)
  8/27/2010, 7:16 PM
Joined 11/21/2007
Last visit: 5/23/2013
Posts: 539
Rating:
Rated: Excellent [4.04 out of 5 / rated 24 time(s)]. (24) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello

I just upgraded my engineering station from PCS7 V7.1 to PCS7 V7.1 + SP1.

After the upgrade, when I open my project and compile the same, I get the error msg. :

HARDWARE ERROR: FIle not Found

...\s7asrcom\00000001\setparameterassignment.scl

Error Msg Attached.herewith.

Any idea, what could be the problem ?

Thanks

Navnag

Attachment: Error.zip  (15 Downloads)

There is no such thing as the last bug in a program
There are no stubborn bugs, There are only stubborn Debuggers.

Top
  8/27/2010, 7:35 PM
Joined 9/27/2006
Last visit: 5/25/2013
Posts: 3953
Rating:
Rated: Excellent [4.15 out of 5 / rated 620 time(s)]. (620) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Navnag;
Sorry, no I don't have a specific answer to your problem.
But users have enquired as to why some charts are lost, or hardware configurations don't seem to upgrade with this migration 9the Search box shows a few threads on the subject).
Have you seen this document, on the procedures to upgrade to SP1?
http://support.automation.siemens.com/WW/view/en/39980937
Hope it helps,
Daniel Chartier



=== Edited by O_Moderator @ 9/16/2010 2:07 PM [GMT ] ===
link edited

Top
  8/27/2010, 8:07 PM
Joined 11/21/2007
Last visit: 5/23/2013
Posts: 539
Rating:
Rated: Excellent [4.04 out of 5 / rated 24 time(s)]. (24) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear dchartier

Thanks . However I have seen this document and followed the instructions in the same.
But problem still remains.

We have even tried to uninstall PCS7 completely and did a clean install of PCS7.1+SP1.

However, we still get the same problem.

The original project works fine in PCS7 V7.1 without problems

Cheers

Navnag

There is no such thing as the last bug in a program
There are no stubborn bugs, There are only stubborn Debuggers.
Top
  7/4/2012, 2:13 PM
Joined 10/8/2005
Last visit: 5/21/2013
Posts: 33
Rating:
Rated: Excellent [5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Navnag,
I have the same problem but I didn't upgrade PCS7, I had PCS7 V7.1 SP2 from the start of my project and I compile my project without error priviouse. But now I added some new CFC and errors same as your error appears and compilation terminated.
Do you find any solution for the problem?
Top
  7/5/2012, 1:35 PM
Joined 2/24/2011
Last visit: 5/24/2013
Posts: 678
Rating:
Rated: Excellent [4.45 out of 5 / rated 58 time(s)]. (58) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

try to delete all blocks from author ES_MAP, also the CFC charts with @....
Recompile you project (delta load will not be possible anymore).

Reorganize your project.

Try this steps and please give feedback.



=== Edited by Silent Bob @ 7/5/2012 1:36 PM [GMT ] ===


=== Edited by Silent Bob @ 7/5/2012 1:36 PM [GMT ] ===


=== Edited by Silent Bob @ 7/5/2012 1:35 PM [GMT ] ===


Top
  7/6/2012, 5:22 PM
Joined 10/8/2005
Last visit: 5/21/2013
Posts: 33
Rating:
Rated: Excellent [5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Silent Bob,
I did your recommended way another time( I had done it before) but it didn't work and compilation terminated in the middle.
I have explained the problem with detail in anaother thread:
 http://www.automation.siemens.com/WW/forum/guests/PostShow.aspx?PageIndex=1&PostID=387132&Language=en
 another question what does it mean " delta load"? what feature I lose if I don't do delta load anymore?
Top
  7/9/2012, 2:11 PM
Joined 2/24/2011
Last visit: 5/24/2013
Posts: 678
Rating:
Rated: Excellent [4.45 out of 5 / rated 58 time(s)]. (58) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

delta laod means that the changes are loaded to the AS without stopping the program.
If you can't delta load, you have to make a complete download of the program, that means, that the AS is going to stop.
Sometimes this isn't possible, e.g. when the production is running.

I will check your problem again.

So far....
Top
  7/9/2012, 2:45 PM
Joined 2/24/2011
Last visit: 5/24/2013
Posts: 678
Rating:
Rated: Excellent [4.45 out of 5 / rated 58 time(s)]. (58) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hi,

I cross checked the other topic you mentioned....
So far, I don't have any idea what it could be, hence you tried everything i normaly would suggest.

Maybe your project is broken.

Try this (please make backup archive before):
- create new CPUs in you project (to replace the existing ones)
- make the HW config like the old ones (don't use export/import configuration)
- maybe adapt the range of FBs and DBs (according old CFC config)
- copy all symbols into new program
- now copy alls CFCs into the new program, and delete the old CPUs

Good luck.
Please give feedback if it helped.

Top
  7/10/2012, 5:52 AM
Joined 10/8/2005
Last visit: 5/21/2013
Posts: 33
Rating:
Rated: Excellent [5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,
Thank you for your anwers and guidelines.
I had a backup from two day before of my broken project an it works ok. Then I work on this backup file and complete it and now it compile correctly. but sometimes when I want to compile the same errors appear. then I exit the CFC and sometimes exit the Simatic Manager. the second time it recompiled correctly without error.
do you have any idea about it?
do you think this problem started from a PC problem for example a Virus? Because when I saw this problem I scanned my computer and the Virus scanner found Stuxnet on one of my archived project and removed the virus. ( I had Microsoft Security and NOD32 on my laptop).

Top
  7/10/2012, 11:50 AM
Joined 2/24/2011
Last visit: 5/24/2013
Posts: 678
Rating:
Rated: Excellent [4.45 out of 5 / rated 58 time(s)]. (58) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi.

Either your project is damaged (also before), or the problem depends on the installation of windows and / or PCS 7 itself.

Have you tried the workaround with the new CPUs?



If I would find a virus... espacially Stuxnet, I would do following.

Wipe the computer completely (using wiping tool, like Deriks Boot and Nuke).

Reinstall everything....

Clean the project on another computer, or inside VMware. Cross check against virus.

And then, if you are shure your project is clean, unzip it on the computer.

Ragarding Stuxnet / IT security read this FAQ: http://support.automation.siemens.com/WW/view/de/43876783
Top
12» Page 1 of 2 (14 items)
Actions