SINAMICS
Using VAC in inputs of Sinamics DCM
Thread Starter: Ssal Started: 7/10/2012 6:19 AM Replies: 0

7/10/2012, 6:19 AM
|
Joined 5/21/2012
Last visit: 10/4/2012
Posts: 1
Rating:
(0)
|
(0)
|
Hi!
I have an application were i insert a tachometer in the main actual value input (XT1.103-.104) of the Sinamics DCM. The problem i have is that the tachometer outputs only alternative current. I'm wondering does the input in DCM suport AC? By using parameter p50743 i can create absolute value of the input, so the scaling is not a problem. And the device were the tachometer is installed only rotates in one direction, so i won't need direction data. I quess the question is mainly about the electronics of the DCM and its inputs? Do they work with AC, or do i have to find a alternative way to solve the dilemma.
Thanks in advance!
|
|
|
|
Actions