Technical Forum

SIMATIC WinCC (TIA Portal)

TIA Compilation Error

Thread Starter: soju   Started: 7/2/2012 12:39 PM   Replies: 9

« Previous thread Next thread »
Page 1 of 1 (10 items)
  7/2/2012, 12:39 PM
Joined 11/29/2011
Last visit: 6/16/2013
Posts: 65
Rating:
Rated: Above avarage [3 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
During the runtime simulation of WINCC V 11  its throwing following error.....

Compailation of the RUNTIME PROJECT FAILED.   Cannot link the database to the runtime project 11866113-9902




Cannot link database to the runtime project.


Thanks,

Soju

Attachment: New Picture.jpg  (14 Downloads)

Top
  7/2/2012, 5:20 PM
Joined 9/5/2011
Last visit: 6/19/2013
Posts: 2736
Rating:
Rated: Outstanding [3.8 out of 5 / rated 136 time(s)]. (136) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Can you described more about your behaviour?
What did you do before?
Which panel do you use?
Which software version do you use?

You can delete the "IM" folder in your project directory.
Then you generate your project new.


Tweety
Top
  7/3/2012, 9:34 AM
Joined 11/29/2011
Last visit: 6/16/2013
Posts: 65
Rating:
Rated: Above avarage [3 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Its Simantic PC Station I am using.  I just created a small design and thought of simulating it in runtime and showing this error. Even without any objects in the Screens also its showing the same error. And today I contacted my local supplier and they are saying its problem with the nstallation so I repaired my installation and it shows some SQL error in installation. Is it because of that its not going to run time. Attached the error log file also..Please check and please help


Thanks,

Soju
Top
  7/3/2012, 9:41 AM
Joined 11/29/2011
Last visit: 6/16/2013
Posts: 65
Rating:
Rated: Above avarage [3 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
ResourceProperty: TermMessage32 = 'Please remove the "WinCC" instance of the SQL Server because it still exists in an incompatible version for WinCC Professional V11.0 SP2 after a deinstallation of "WinCC Professional" or "WinCC Runtime Professional".\n\n' (RawValue: 'Please remove the "WinCC" instance of the SQL Server because it still exists in an incompatible version for [BUNDLETITLESHORT] after a deinstallation of "WinCC Professional" or "WinCC Runtime Professional".\n\n') 11:38:20|.         |Installer::InitInstaller                |(01




Acoording to this I had unisntalled all the TIA instances and installed it again but still the same.

Thanks,

Soju
Top
  7/3/2012, 11:40 AM
Joined 9/5/2011
Last visit: 6/19/2013
Posts: 2736
Rating:
Rated: Outstanding [3.8 out of 5 / rated 136 time(s)]. (136) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Have you check this behaviour with a new project?

Do you make a repair installation and the behaviour is the same?

Do you deinstall WinCC V11 and install it new.
Have you done this?

Tweety
Top
  7/3/2012, 12:58 PM
Joined 11/29/2011
Last visit: 6/16/2013
Posts: 65
Rating:
Rated: Above avarage [3 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Yes created new project also same error.

Done uninstall/ install same error.



Please find the attached error log while installing the wincc again.

Installation completed with the following error log report.

I had done the repair, reinstallig but still while compiling showing the same error


Thanks,

Soju

Attachment: SIA_WINCC_PROFESSIONAL_V11.zip  (9 Downloads)



=== Edited by soju @ 7/3/2012 1:00 PM [GMT ] ===



Top
  7/4/2012, 1:32 PM
Joined 9/5/2011
Last visit: 6/19/2013
Posts: 2736
Rating:
Rated: Outstanding [3.8 out of 5 / rated 136 time(s)]. (136) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Do you use the right operating system for WinCC V11?

You find the list of software on the end of this FAQ.
With what is SIMATIC WinCC V11 compatible?

You should check the software of your computer with this list.


Tweety
Top
  7/6/2012, 6:03 AM
Joined 11/29/2011
Last visit: 6/16/2013
Posts: 65
Rating:
Rated: Above avarage [3 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi Tweety,


I am using Windows 7 Enterprise Edition and I checked the compatability too.

Thanks, 

Soju
Top
  7/6/2012, 12:29 PM
Joined 9/5/2011
Last visit: 6/19/2013
Posts: 2736
Rating:
Rated: Outstanding [3.8 out of 5 / rated 136 time(s)]. (136) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

In this case, you should start a support request on the customer support.
---> customer support

Tweety
Top
  7/16/2012, 6:57 AM
Joined 11/29/2011
Last visit: 6/16/2013
Posts: 65
Rating:
Rated: Above avarage [3 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi Tweety,

My issue got solved. There is some wrong instance of SQL service running in my machine. Thats why....So when ever I am installing TIA portal SQL installation is not proper thats why getting this error.

Done formating and installed TIA again and the installation is perfect and project running fine.


Thanks for all your support
Top
Thank you for this post from:
Page 1 of 1 (10 items)
Actions