Technical Forum

LOGO!

Basic vs pure

Thread Starter: acik   Started: 7/4/2012 5:12 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  7/4/2012, 5:12 PM
Joined 6/20/2012
Last visit: 4/18/2013
Posts: 12
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
What is the difference ?
Top
  7/5/2012, 8:04 AM
Joined 4/22/2010
Last visit: 5/18/2013
Posts: 3190
Rating:
Rated: Excellent [4.11 out of 5 / rated 295 time(s)]. (295) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Basic is with display and Pure without display.

That's all.

Manual wrote:


Which devices are available?
LOGO! Base Modules are available in two voltage classes:
● Class 1 ≤ 24 V, i.e. 12 V DC, 24 V DC, 24 V AC
● Class 2 > 24 V, i.e. 115...240 V AC/DC
LOGO! Base Modules are available in two versions:
● LOGO! Basic (version with display): 8 inputs and 4 outputs
● LOGO! Pure (version without display): 8 inputs and 4 outputs
Each version is integrated into four (if 0BA6) or six (if 0BA7) subunits, is equipped with an
expansion interface and LOGO! TD interface and provides 39 (if 0BA6) or 44 (if 0BA7) preconfigured
standard and special function blocks for the creation of your circuit program.


Regards,

Marcjan



=== Edited by Marcjan @ 7/5/2012 8:23 AM [GMT ] ===



Problem solved?
Please let us know!

Please no technical questions by PM, use the forum!
Top
Page 1 of 1 (2 items)
Actions