Technical Forum

STEP 7 Additional Software

Hardware error: FILE_NOT_FOUND (1739:10) during compiling of safety program

Thread Starter: Farzad   Started: 7/4/2012 1:59 PM   Replies: 9

« Previous thread Next thread »
Page 1 of 1 (10 items)
  7/4/2012, 1:59 PM
Joined 10/8/2005
Last visit: 5/21/2013
Posts: 33
Rating:
Rated: Excellent [5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear All Users,
I have developed a safety program in CFC. my CPU is S7-417F/FH. Previously I had developed 4 fail safe CFC  and 2 standard CFC in my project and compiled it without any errors. after some day I added 6 fail safe CFC to my project. after that when I compile my project an error message with the following text apears and terminated the compiling procedure.
"Compile chart as block type (1739:10)"
" Hardware error : FILE_NOT_FOUND"
" d:\My_Prj\s7asrcom\00000001\forceswitch.scl"

I try many times and do alot of procedures such as "Reorganize" the project , delete all CFC that are created automatically and recompile and ... but all the time I am confronted with the above error.
in addition some time the error appears for another file in the same folder for example for "setparamassignment.scl" and "castingassignmentcode.scl" file.

Is there anybody tell me whats the problem?

picture of the error is in the attachment.

Attachment: error.JPG  (23 Downloads)

Top
  7/4/2012, 2:18 PM
Joined 8/10/2011
Last visit: 5/3/2013
Posts: 9
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

dear farzad

you should check when you copy the new failsafe block form other project to privouse the name of block including header and symbolic name change or not the , then if you find you should change it ,all relative blocks must be copy to new project.

Top
  7/4/2012, 7:41 PM
Joined 10/8/2005
Last visit: 5/21/2013
Posts: 33
Rating:
Rated: Excellent [5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi turbomedia,
I didn't copy fail safe block from other project. I create my own F block type and I tested it in fail safe  CFCs of project and it works properly. but after adding some CFCs to my project it doesn't work and doesn't compile completely.

Top
  7/5/2012, 6:33 AM
Joined 8/10/2011
Last visit: 5/3/2013
Posts: 9
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
dear farzad

first of all let me to know , what is the version of previouse & latest the CFC?, because i wanna to know you have mismaching between two available version , i guess when you were upgrading the CFC some hardware configuration missing or didnt updating.


Top
  7/5/2012, 12:01 PM
Joined 10/8/2005
Last visit: 5/21/2013
Posts: 33
Rating:
Rated: Excellent [5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi turbomedia,
I had created all of CFCs in the same version. I had CFC Editor version V7.1+SP2.
and all of CFCs created in this version.
Top
  7/30/2012, 12:48 PM
Joined 10/8/2005
Last visit: 5/21/2013
Posts: 33
Rating:
Rated: Excellent [5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear all,
the same problem appeared when I compile " entire program" but when I compile "only changes" it compiled correctly!!!!!????.

Top
  7/30/2012, 3:29 PM
Joined 9/5/2011
Last visit: 5/22/2013
Posts: 32
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello farzad,

please have a look on this article!

Maybe it would be interesting or helpful for you!blink

http://support.automation.siemens.com/WW/view/en/34468224

Greetings,

mika

Top
  8/4/2012, 2:23 PM
Joined 10/8/2005
Last visit: 5/21/2013
Posts: 33
Rating:
Rated: Excellent [5 out of 5 / rated 2 time(s)]. (2) 
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Hi all,
Finally I found where is the problem. I used Microsoft Essential Security on my laptop. I uninstalled this damn antivirus! and now everythings are OK.
Thanks all
Top
Thank you for this post from:
  10/8/2012, 1:09 PM
Joined 2/18/2009
Last visit: 12/14/2012
Posts: 11
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thank you so much for the update!

I had same problem as well, but I will try to exclude the project library from the security essential.

And I couldn't believe my eyes when I saw that this post was updated with the answer to the problems.


Thanks againRnf:lblSmileyTooltip_
Top
Thank you for this post from:
  3/6/2013, 8:39 AM
Joined 8/26/2008
Last visit: 5/25/2013
Posts: 5
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi All,

               I had the same problem with Compilation and after i saw this solution in the Forum am happy. I just disabled Virus & Spyware Protection and able to Compile without any problem.Rnf:lblSmileyTooltip_


              Anyway thanks Mr.Farzad.Rnf:lblSmileyTooltip_

Thanks&Regards,
Puvvadi
Top
Thank you for this post from:
Page 1 of 1 (10 items)
Actions