Technical Forum

Communication / Networks

how to make a modbus communication with the ET200 6es7 138 4df11 0AB0?

Thread Starter: Jefferson Almeida   Started: 7/2/2012 9:18 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  7/2/2012, 9:18 PM
Joined 7/2/2012
Last visit: 5/14/2013
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

I'm having some difficulties in the module configuration. Well I tried several ways to do this setup but got no results. I'm using a library available for download and manual setting available in the same site. The LED module Modbus / USS do not light the tx and rx with it I do not know where the problem is, I'm new to this type of application and am encountering many difficulties in the creation of DBs that will obtain the data.

If they have, I need an example application for this type of communication, I'm testing with equipment that communicated in other Modbus PLCs and it worked perfectly.

graciously

Sorry for bad English

Jefferson

Top
  7/4/2012, 5:52 PM
Joined 11/27/2007
Last visit: 5/23/2013
Posts: 843
Rating:
Rated: Outstanding [3.86 out of 5 / rated 58 time(s)]. (58) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Jefferson,
an example is available:
Function Blocks, Examples and User Manuals of the Serial Interface ET200S 1SI

Regards,
Kaulquappe
Top
Page 1 of 1 (2 items)
Actions