Technical Forum

SIMATIC S7-300 / S7-300F

S7300 instead of S7-400 CPU

Thread Starter: apesky   Started: 7/2/2012 10:02 AM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  7/2/2012, 10:02 AM
Joined 9/5/2011
Last visit: 7/2/2012
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,
We are working in cement industry and we want to upgrade our existing ESP filter with a new bag filter. We have an existing PCS7 system in our plant and we asked to the companies to use a new S7-300 PLC for this small project including one new workstation for the operator. (In the plant we use SIMATIC PCS7 V6.1 Engineering PowerPack (AS/OS PO 3000)).
The company answered me that we can not use S7-300 within this project as it is not compatible with PCS7 V6.0. Is this true? For my knowledge both S7-300 nad S7-400 CPUs use same step7 software.

[schnippschnapp]

Thanks in advance for supports.

Best regards,
Atilla YILDIZ



=== Edited by O_Moderator @ 7/3/2012 10:44 AM [GMT ] ===
second question is splitted to CEMAT V.6.1 license

Top
  7/2/2012, 10:36 AM
Joined 10/7/2005
Last visit: 5/20/2013
Posts: 2353
Rating:
Rated: Excellent [4.26 out of 5 / rated 612 time(s)]. (612) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello apesky
apesky wrote:
The company answered me that we can not use S7-300 within this project as it is not compatible with PCS7 V6.0. Is this true?

it's half true I'd say and perhaps there is just a bit of a misundestanding.
PCS7 is based on S7-400 usage, but you can nonetheless sort of "integrate" an S7-300 into a PCS7 based system and below is the info on what to consider and do in this case:
S7-300 / S7-400 Package Unit Integration in SIMATIC PCS 7

Having said, have you considered to simply expand your PCS7 system with a remote I/O station for this purpose and let your existing (PCS7 engineered) S7-400 do the logic?

[schnippschnapp]

I hope this helps




=== Edited by O_Moderator @ 7/3/2012 10:44 AM [GMT ] ===



Cheers

fritz

The advice and opinion given in this thread is that of the author and does not necessarily reflect the views of I S Systems Pty Limited.
To find out how I S Systems can help you with your automation needs please visit www.issystems.com.au.
Top
  7/2/2012, 11:17 AM
Joined 9/5/2011
Last visit: 7/2/2012
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi Fritz,
Thanks for information.
Our idea is to use S7-300 not only as a remote IO but main controller for the logic and we want to connect it to existing PCS7.
The company says this is not possible and we have to use S7-400 for the logic(then remote IO will be S7-300 modules) as S7-300 is not compatible with PCS7 engineering system.

[schnippschnapp]

Cheers
Atilla



=== Edited by O_Moderator @ 7/3/2012 10:45 AM [GMT ] ===


Top
Page 1 of 1 (3 items)
Actions