SIMOTICS
spindle motor 1PH7163-2ND23-0BC0
Thread Starter: Zlatkodo Started: 6/29/2012 7:47 AM Replies: 2

6/29/2012, 7:47 AM
|
Joined 6/29/2012
Last visit: 7/3/2012
Posts: 4
Rating:
(0)
|
(0)
|
Siemens spindle motor 1PH7163-2ND23-0BC0 We need to rewind this motor (probably is 22 kW, 4 pole winding) but we have only empty stator core with no nameplate or winding data . Motor run trough the controller SIMODRIVE 611 , ( 0 to 1400 Hz at pulse frequency 3.2kHz). We need help with all nameplate data, especially : rated frequency and voltage, connection and duty cycle ( for example: 400 V, 50 Hz, Y, S1). BTW, the best help would be to obtain all the winding data, if possible. Thanks in advance. Zlatkodo opetja@ymail.com
=== Edited by Zlatkodo @ 6/29/2012 7:49 AM [GMT ] ===
|
|
|
|
|

7/3/2012, 1:29 PM
|
Joined 10/11/2006
Last visit: 5/22/2013
Posts: 755
Rating:
(78)
|
(1)
|
Hello,
I think it's not too easy to rewind such a motor 
Attached a figure of the motor parameters.
Good luck
Best regards
TechTeam
|
|
|
|

7/3/2012, 6:59 PM
|
Joined 6/29/2012
Last visit: 7/3/2012
Posts: 4
Rating:
(0)
|
(0)
|
Thanks for useful data. Seems to me, it's impossible to get the manufacturers winding details (number of turns per coil, wire size...). Zlatkodo
|
|
|
|
Actions