Hello,
it will be a difference. Unfortunately I can not find the 1LP4209. But the difference will be the rated power.
For example:
1LP4204-4CA91
LOW-VOLTAGE MOTOR, IEC
SQUIRREL-CAGE,SELF-COOLED,IP55
FOR HOISTING APPLICATIONS
TEMP. CL. 155(F) USED AS CL. F
CAST IRON HOUSING * FS200L
4POLE * S3-25% * 45KW(50HZ)
52KW(60HZ)
NON-STANDARD WINDING
3 AC ..HZ, ...V, ...KW
IM B 5, IM V1 W/O CANOPY
FLANGE: FF350FLANSCH: FF350
1LP4208-4CA91
LOW-VOLTAGE MOTOR, IEC
SQUIRREL-CAGE,SELF-COOLED,IP55
FOR HOISTING APPLICATIONS
TEMP. CL. 155(F) USED AS CL. F
CAST IRON HOUSING * FS200L
4POLE * S3-25% * 37KW(50HZ)
42,5KW(60HZ)
NON-STANDARD WINDING
3 AC ..HZ, ...V, ...KW
IM B 5, IM V1 W/O CANOPY
FLANGE: FF350
Best regards
TechTeam