Technical Forum

SINUMERIK / SIMODRIVES / MASTERDRIVES / SIMOTION / SINAMICS

Energy conservation system for plant

Erstellt von RAJKIRAN am 15.05.2012 13:14 (5 Antworten)

« Vorheriges Thema Nächstes Thema »
Seite 1 von 1 (6 Objekte)
  15.05.2012, 13:14
Beigetreten am: 18.08.2009
Letzter Besuch: 17.04.2013
Beiträge: 464
Bewertung:
Bewertung: Herausragend [3,63 von 5 / 32 mal bewertet]. (32) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Dear Expert,
 I want to used energy conservation system for plant by using Suitable drive...
I have all Pump/Motor's Power rating(in KW & HP),current rating & starter type of whole plant....
I want to know any extra I/P required from above list for energy conservation system.
Also tell me if there is any important doc. so that by using this doc. I can establish total energy conservation system & send energy conservation system PPT.


Rajkiran Patil

Executive Project Eng r.- Process Automation


Top
  16.05.2012, 10:12
Beigetreten am: 08.07.2009
Letzter Besuch: 17.05.2013
Beiträge: 1167
Bewertung:
Bewertung: Exzellent [4,25 von 5 / 326 mal bewertet]. (326) 
Bewertung: Exzellent [4,25 von 5 / 4 mal bewertet]. (4) 

RAJKIRAN wrote:
Dear Expert,

 I want to used energy conservation system for plant by using Suitable drive...

I have all Pump/Motor's Power rating(in KW & HP),current rating & starter type of whole plant....

I want to know any extra I/P required from above list for energy conservation system.

Also tell me if there is any important doc. so that by using this doc. I can establish total energy conservation system & send energy conservation system PPT.

 



Hello Rajkiran,

Energy Conservation System is really Big thing and that too if your Plant is Big

As first step, you need to study every Load which are very much cruical and have a huge part in total consumption, then you need to workout to reduce consumption for same

You need Power Rating, and application detail to select any Drive. Replacing so many DOL/SoftStarter with Drives will be result in to Heavy investment at Start so you have to Optimise between all this

Using Drive For every direct motor, will result in to Energy Saving

You can think out of using Different features of Drive for saving Energy, like use of PID in Compressor

Another thing you is constant power/load monitoring System in your Plant

Regards
Devesh




=== Edited by Vithani @ 5/16/2012 5:28 PM [GMT ] ===



Please say Thanks if your Problem is Solved.. :-)
Top
Für diesen Beitrag bedankt sich:
  17.05.2012, 07:35
Beigetreten am: 18.08.2009
Letzter Besuch: 17.04.2013
Beiträge: 464
Bewertung:
Bewertung: Herausragend [3,63 von 5 / 32 mal bewertet]. (32) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Thanks Vithani,
could you provide any doc. regarding this so this will help me...

Rajkiran Patil

Executive Project Eng r.- Process Automation


Top
  17.05.2012, 20:43
Beigetreten am: 29.12.2011
Letzter Besuch: 07.06.2012
Beiträge: 32
Bewertung:
Bewertung: Exzellent [4,25 von 5 / 4 mal bewertet]. (4) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Here is a link to a really good writeup on Energy conservation using VSD's

http://oee.nrcan.gc.ca/industrial/equipment/variable-frequency-drives/17167


Best Regards
Mr_Al
Top
  25.05.2012, 22:03
Beigetreten am: 28.04.2010
Letzter Besuch: 08.03.2013
Beiträge: 58
Bewertung:
Bewertung: Exzellent [4,56 von 5 / 16 mal bewertet]. (16) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Dear Rajkiran,

You can use Sinasave software for estimation of energy conservation by using drives.
Please download sinasave from www.siemens.com/sinasave.

Alternatively you can use Sizer web engineering for the same purpose.
Please visit the following link.
https://www.automation.siemens.com/sizer-ld/Pages/SinaSave/StartSinaSave.aspx

These tools are excellent for estimating energy saving for different loads in an industry.

Regards
Ajay Gupta
  
Top
  26.06.2012, 15:12
Beigetreten am: 25.06.2012
Letzter Besuch: 29.06.2012
Beiträge: 5
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
RAJKIRAN wrote:
Dear Expert,
 I want to used energy conservation system for plant by using Suitable drive...
I have all Pump/Motor's Power rating(in KW & HP),current rating & starter type of whole plant....
I want to know any extra I/P required from above list for energy conservation system.
Also tell me if there is any important doc. so that by using this doc. I can establish total energy conservation system & send energy conservation system PPT.



It really is a big thing tight now to use energy conservation for plants. I started using it for my own plants from serenata online uk and it works really great so far. I had someone coming over to explain me the whole procedure of energy conservation and he also handed me a manual for the correct utilization.
Top
Seite 1 von 1 (6 Objekte)
Aktionen