Technical Forum

SIMOTICS

Classes of motors

Thread Starter: Nishant007   Started: 6/25/2012 11:52 AM   Replies: 5

« Previous thread Next thread »
Page 1 of 1 (6 items)
  6/25/2012, 11:52 AM
Joined 6/22/2012
Last visit: 7/24/2012
Posts: 5
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hie
What exactly the classes of motors are?
How the classes of motors is defined?

Top
  6/26/2012, 2:56 PM
Joined 10/11/2006
Last visit: 5/17/2013
Posts: 744
Rating:
Rated: Outstanding [3.97 out of 5 / rated 78 time(s)]. (78) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

what do you mean with classes ? Please define it more clearer.

Best regards
TechTeam
Top
  6/28/2012, 8:00 AM
Joined 4/28/2010
Last visit: 3/8/2013
Posts: 58
Rating:
Rated: Excellent [4.56 out of 5 / rated 16 time(s)]. (16) 
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 
Dear Nishant,

The classes of motor refers to the classification based on insulation and temperature rise limit of the motor.

Please refer the attached informative pages on your topic.

Regards,
Ajay Gupta

Attachment: AG05 (Temperature Rise).pdf  (23 Downloads)

Top
  7/12/2012, 7:54 AM
Joined 6/22/2012
Last visit: 7/24/2012
Posts: 5
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Sir,

 I want to know how you define classes of motors like(class 5, class 10, class 15, class 20)?????
based on these classes  we define triping in numerical relays.
Top
  7/18/2012, 2:24 PM
Joined 10/11/2006
Last visit: 5/17/2013
Posts: 744
Rating:
Rated: Outstanding [3.97 out of 5 / rated 78 time(s)]. (78) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

I'm not sure if I understand but we have motor side no classes like 5, 10... like for the relays. We have classes for the temperature rise limit like Ajay Gupta has said. But other classes ?

Best regards
TechTeam
Top
  7/20/2012, 1:32 PM
Joined 4/23/2010
Last visit: 5/17/2013
Posts: 1148
Rating:
Rated: Outstanding [3.17 out of 5 / rated 53 time(s)]. (53) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Nishant007 wrote:
Dear Sir,

 I want to know how you define classes of motors like(class 5, class 10, class 15, class 20)?????
based on these classes  we define triping in numerical relays.


Hello,
Basically motors are manufactured on basis of power rating, RPM, duty cycle, insulation class, type of mounting, etc. Relays i.e. protection relays are selected upon the class or type of protection desiered, e.g. class 5, class 10 etc. So the general purpose manufactured motor may have class 5 or class 10 protection relay selected by the end user depedening upon the application & protection desiered by end user.

Tell me and I will forget. Show me and I will remember. Involve me and I will understand. -Confucius
Top
Page 1 of 1 (6 items)
Actions