Technical Forum

SINUMERIK CNC automation systems

SINUMERIK 880T GA2 PROBLEM IN START

Thread Starter: AGARCIA   Started: 6/21/2012 10:28 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  6/21/2012, 10:28 PM
Joined 3/31/2010
Last visit: 3/1/2013
Posts: 12
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

I' ve a problem in START Sinumerik 880T GA2.

When, Power-up the control  diagnostic on operator panel, appears on the screen

the diagnostic display an error in application BAS-DIO (yellow highlight)

The LEDs on the CPU in the operator panel (OP CPU)   the four LEDs flashing simultaneously on the operator panel.

In Board INT-KEYBORD the led is yellow highlight

In board PLC-CPU the led is on

In board INT/DMP the led in on  

 

I chance the OP-CPU (6SN1120-4BD03) on operator panel.

I check  the connection between the operator panel and NC  (check de cable)

I chance power supply in OP and NC

 

 the error in application BAS-DIO is present.

Can someone help me?


Attachment: Doc2.pdf  (12 Downloads)

Top
  7/21/2012, 10:15 PM
Joined 7/7/2011
Last visit: 5/20/2013
Posts: 16
Rating:
Rated: Excellent [5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
did you initalise the com card on the rear of the monitor? you use the rotary switch on the back
Top
Page 1 of 1 (2 items)
Actions