Technical Forum

SIMATIC TDC, FM458, T400

TDC with thrid party FOC communication.

Thread Starter: DUTTA   Started: 6/20/2012 6:54 PM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  6/20/2012, 6:54 PM
Joined 2/26/2008
Last visit: 3/14/2013
Posts: 97
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Experts,

Can you clarify following doubts:

1) Fastest scan/execution time for TDC processors. Can TDC configure to have a cyclic interupt for 65 MicroSeconds (Very few instruction are required to execute under this cycle)?

2) Does TDC has any CP or H/W which can talk to Fiber Optic base device? What is that options?


Regards,
Dutta
Top
  6/21/2012, 10:22 AM
Joined 8/31/2005
Last visit: 6/17/2013
Posts: 994
Rating:
Rated: Outstanding [3.85 out of 5 / rated 122 time(s)]. (122) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
DUTTA wrote:

1) Fastest scan/execution time for TDC processors. Can TDC configure to have a cyclic interupt for 65 MicroSeconds (Very few instruction are required to execute under this cycle)?
Hello Dutta,
the minimal task time is 100µs.
DUTTA wrote:

2) Does TDC has any CP or H/W which can talk to Fiber Optic base device? What is that options?
TDC can use a "Global Data Memory" this is connected with a fiber optic to the TDC racks. But the protocoll is not published. The only non TDC component I know is ibaPDA.

mfG / Best Regards

Dirk
Top
  6/21/2012, 6:23 PM
Joined 2/26/2008
Last visit: 3/14/2013
Posts: 97
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Miami,

Thank you for the reply.

1) Can TDC has any i/o based interrupt which can give less then 100micro sencond cycle?

2) Can I develop code to use this FOC module for third party communication? Is any communication block like send/receive available in TDC library?

Reply me.

Regards,
Dutta.
Top
  6/22/2012, 10:54 AM
Joined 8/31/2005
Last visit: 6/17/2013
Posts: 994
Rating:
Rated: Outstanding [3.85 out of 5 / rated 122 time(s)]. (122) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello DUTTA!
  1. As far as I know you can trigger a alarmtask by a digital input. Please note this inputs can have up to 50µs delay. I have no idea if ther will be a jitter. An I expect you can use not more than 10 or 15 blocks.
  2. TDC has no open communication. All kind of communication uses a central communication block (this one is protokoll specific) and universal used send and receive blocks.
    With the D7-FB-Gen you can not write communication blocks.

mfG / Best Regards

Dirk
Top
  10/20/2012, 9:08 AM
Joined 10/20/2012
Last visit: 10/20/2012
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
good topic

wiger
Top
Page 1 of 1 (5 items)
Actions