Technical Forum

Meet & Talk

Gauge with 5 colors

Thread Starter: Import-User-1   Started: 6/18/2012 10:50 AM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  6/18/2012, 10:50 AM
Joined 8/10/2005
Last visit: 5/15/2013
Posts: 3031
Rating:
Rated: Outstanding [3.12 out of 5 / rated 17 time(s)]. (17) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Import of a Technical Question of a unregistered User

Guest wrote:
hello,
for an project i need a gauge which will have 5 colors, lets say 0-20 red, 20-40 yellow, 40-60 green, 60-80 yellow again and 80-100% red again. the standard gauge only supports 3 colors and i have no idea if it is possible to edit the standard gauge.
Top
  6/20/2012, 7:23 AM
Joined 4/8/2011
Last visit: 6/29/2012
Posts: 270
Rating:
Rated: Excellent [4.49 out of 5 / rated 47 time(s)]. (47) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Import-User-1,

I'm not sure if you are using WinCC flexible or TIA Portal, but at least in WinCC flexible (2008) there's an option in properties - general called "Dial graphic", where you can set a custom picture for the gauge circle. Now all you need to do is play a bit with MS Paint or something like that.

Hope this helps.

I don't see why people would still care about travelling salesman problem nowadays. You can simply buy stuff on the internet.
Top
  6/22/2012, 1:31 PM
Joined 10/3/2010
Last visit: 5/17/2013
Posts: 731
Rating:
Rated: Outstanding [3.39 out of 5 / rated 49 time(s)]. (49) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I would create own drawn gauge and use dynamic dialog connected to an external tag. PLC fills value of this tag.
Top
Page 1 of 1 (3 items)
Actions