Technical Forum

SINUMERIK / SIMODRIVES / MASTERDRIVES / SIMOTION / SINAMICS

DC drive conversion

Thread Starter: Patidar   Started: 6/16/2012 12:28 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  6/16/2012, 12:28 PM
Joined 1/5/2012
Last visit: 3/30/2013
Posts: 29
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear all,

I have 6RA24 Drives & want to replace those drives so what would be be better choice 6RA70 or 6RA80?

Please suggest

Regards,

Patidar
Top
  6/16/2012, 11:09 PM
Joined 8/8/2011
Last visit: 5/18/2013
Posts: 119
Rating:
Rated: Outstanding [4 out of 5 / rated 25 time(s)]. (25) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Patidar,

It would be best to replace with 6RA80 drives since they are the most recently developed dc drive product offered by Siemens. 

The 6RA80 drives power modules are available in a variety of different voltages, 2 Quadrant operation, and 4 Quadrant operation. 

Attached is a example page from catalog for SINAMICS DCM Catalog D23.1 for 4 Quadrant Operation at 400 and 480 VAC. 

You may refer to the catalog for your specific product requirements.

https://www.industry.usa.siemens.com/drives/us/en/electric-drives/dc-drives/sinamics-dc-drives/Pages/sinamics-dc-drives.aspx

Expand General Information menu on right side of page to get access to additional information such as catalog, brochures, etc.

Deputy


 

Attachment: DC Converters 4 Quad 400V and 480V.pdf  (15 Downloads)

Top
  6/17/2012, 8:42 AM
Joined 4/24/2009
Last visit: 5/17/2013
Posts: 1948
Rating:
Rated: Outstanding [3.89 out of 5 / rated 100 time(s)]. (100) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thread closed, because question is already published in the following thread Drive conversion from 6RA24 to 6RA70

Best regards
O_Moderator
Top
Page 1 of 1 (3 items)
Actions