LOGO!
SD card capacity
Thread Starter: markheuer Started: 6/15/2012 11:18 PM Replies: 3

6/15/2012, 11:18 PM
|
Joined 3/4/2011
Last visit: 12/11/2012
Posts: 30
Rating:
(0)
|
(0)
|
According to the 0BA7 manual, the 0BA7 can only write 2000 'records' to the SD card. Why is that? I would imagine an 8G SD card could hold quite a bit more.
|
|
|
|
|
Thank you for this post from:
|

6/25/2012, 9:54 AM
|
Joined 7/24/2006
Last visit: 5/24/2013
Posts: 1828
Rating:
(216)
|
(0)
|
Hi,
you are right. Max. Datalog entries is 2000 in one datalog file.
This is limited in the HW and can not be changed.
What you can do is switch RUN/STOP. In this case an additional datalog record will be created on the SD-Card.
Note: Via SW you can only read the latest datalog file from the SD-Card. The other datalog file you can read if you plug in the SD card to a card reader.
How ever, the left memory on the SD card can be used to store other file (Documentation, SP's or any other file).
Hope this helps
|
|
|
|

6/25/2012, 2:08 PM
|
Joined 6/25/2012
Last visit: 6/29/2012
Posts: 5
Rating:
(0)
|
(0)
|
Well though that would appear as something that would not suffice, it actually works for almost available instance.
And to see things fairly, there are a lot of other options that would likely be considered to go on progressively.
By the end of the day, you just have to consider how they are going to work and go on fairly on almost all accounts.
|
|
|
|

7/3/2012, 1:02 PM
|
Joined 7/3/2012
Last visit: 7/3/2012
Posts: 1
Rating:
(0)
|
(0)
|
The Max entry is 2000. We cant change it.
Regards,
|
|
|
|
Actions