Technical Forum

Communication / Networks

AS-I, control word for Movimot ASI of SEW

Thread Starter: miguel.rodrigues   Started: 6/15/2012 5:27 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  6/15/2012, 5:27 PM
Joined 6/15/2012
Last visit: 12/13/2012
Posts: 8
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello to everybody,

I need help with AS-Interface.

I have a MOVIMOT (SEW) with AS-I and a PLC 315-2DP (SIEMENS) and CP343-2P card (SIEMENS).
I need make the motor move, but i dont know how to do for startup the motor.
I need control word, speed and ramp.
Somebody have a exemple (little FC block)?

Somebody can help?

Thanks a lotRnf:lblSmileyTooltip_
Top
  6/15/2012, 8:48 PM
Joined 9/27/2006
Last visit: 5/20/2013
Posts: 3932
Rating:
Rated: Excellent [4.15 out of 5 / rated 619 time(s)]. (619) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Miguel;
Do you have a copy of the Movimot operating manual?

http://www.sew-eurodrive.de/download/pdf/16817613.pdf

I have etracted basic information on the AS-interface connectioon: there are 2 options, one that gives you digital control (using combination of bits and potentiometer settings on the drive) and the other (double-slave) that allows you to write a speed reference and a control word.

Hope this helps,
Daniel Chartier

Attachment: SEW AS-i.JPG  (16 Downloads)

Top
  5/16/2013, 9:16 AM
Joined 5/9/2013
Last visit: 5/19/2013
Posts: 7
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi Miguel,

I did a screeshot from the MoviMot AS-I manual which Dan attached.

that's simple way to make the drive to run by data bits. wish it may help.

Cheers, 

Attachment: SEW_MoviMot_AS-I.JPG  (1 Downloads)

Top
Page 1 of 1 (3 items)
Actions