Hi all!
I have a CPU 414 and a module AO 8 x 13 bit and I'm trying to send a 4-20mA signal to a position controller which controlles the position of a hydraulic cylinder. I used fc106 to convert a value from mm to a scale from 0 to 27648. I changed the 8 AOs from V to A. And I wrote at the OUT of FC106: PAW512 where the address of the first analog output is. I think that PAW512 is wrong. How can I send a value between 0 and 27648 directly to an analog output? I don't see any LED of this module (6ES7432-1HF00-0AB0) lighting. Why? If I send a value to an AO, 13800 for example, should this send approximately 12mA to the controller, right?
Thanks for your help in advance,
Sotos