Technical Forum

SIMOVERT MASTERDRIVES

braking unit

Thread Starter: Amit3545   Started: 6/11/2012 8:09 AM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  6/11/2012, 8:09 AM
Joined 2/27/2012
Last visit: 5/7/2013
Posts: 16
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 


I have Air-cooled Power Module in chassis format 110 Kw ( 6SL3310-1TE32-1AA3 ) which is sinamic series.
Can i used braking unit of master drive(6SE7032–7EB87–2DA0) which have braking power 170 KW?

thanks,
Amit
Top
  6/13/2012, 12:13 AM
Joined 8/8/2011
Last visit: 5/20/2013
Posts: 120
Rating:
Rated: Outstanding [4 out of 5 / rated 25 time(s)]. (25) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Amit,

Yes, you may use these part numbers together to dissipate regenerative energy since they match in voltage range for dc voltage link, but also must have appropriate sized braking resistor according to resistance and power rating for the braking unit.

Deputy
Top
Page 1 of 1 (2 items)
Actions