SIMATIC S5 / STEP 5
Synchronisation between 928B CPU and CP5431
Thread Starter: KG* Started: 6/7/2012 2:26 PM Replies: 2

6/7/2012, 2:26 PM
|
Joined 12/20/2011
Last visit: 5/22/2013
Posts: 13
Rating:
(0)
|
(0)
|
Dear all,
My basic requirement is that i want to synchronise CPU 928B and CP5431(6GK1543-1AA01). I have the basic things like, I have written a program where i have called FB126 (send all) and FB127 (receive all) in OB1. I have called FB125 (SYNCHRON) block in OB20, OB21, OB22 and assigned proper parameters to it, i.e. I have set SSNR = 0 and the base SSNR set in CP5431 is also 0. The same CPU program is working fine with CP1430 and i have established communication between S5 CPU and WinCC over ethernet.For both communications(CP1430, CP5431) the CPU goes in run state. And I dont think there is any problem in CPU program. But i am facing problem in CP5431.
Coming to CP5431, i am using the COM5431E package for programming the CP. I have referred the "FDL connection over PROFIBUS between PC station and SIMATIC S5" and programmed the CP accordingly. But when i put the CP from stop to start, the STOP LED is lit continuously while the green LED lits up only for a few seconds, after that only the STOP LED glows. After this i am not able to access the CP. When i ask for CP status i get an error as "CP interface not ready".
Please can any one help me sort out this problem.
Thanking in advance.
|
|
|
|

6/7/2012, 4:16 PM
|
Joined 7/18/2011
Last visit: 5/24/2013
Posts: 278
Rating:
(31)
|
(0)
|
Hi KG*
What is the SSNR of CP1430 card ? If it is also set to zero, you'll have to choose another (free) one for your CP5431 card. Did you checked if your CP is inserted in a slot that is suited for this CP card ?
Kind regards, BV
|
|
|
|

6/8/2012, 6:03 AM
|
Joined 12/20/2011
Last visit: 5/22/2013
Posts: 13
Rating:
(0)
|
(0)
|
Hello BeVee,
The communication with WinCC using CP1430 card was done seperately. After this I removed the CP1430 card and used the same CPU program for CP5431. The SSNR in CPU program was kept as 0 while the Base SSNR in CP program was also 0. And the slot where i have inserted the CP5431 card is for CP. I tried on other CP slots as well but no success.
|
|
|
|
Actions