Technical Forum

Communication / Networks

Ping a device from S7 program an ehternet device

Thread Starter: Cheeko   Started: 6/6/2012 4:09 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  6/6/2012, 4:09 PM
Joined 5/24/2010
Last visit: 5/1/2013
Posts: 15
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,


Is there a block in S7 where an ethernet device We can ping to know if the device is available?
The device is on the same network as CP443-1 is connected to 

Cheeko
Top
  6/7/2012, 11:45 PM
Joined 3/1/2012
Last visit: 4/12/2013
Posts: 33
Rating:
Rated: Excellent [4.33 out of 5 / rated 6 time(s)]. (6) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Have a look at:

http://support.automation.siemens.com/WW/view/en/30564821

wrote:

2.3.2  AG_CNTEX

● Send PING command (expansion compared with AG_CNTRL)
You can check whether a specific node is reachable in the networ

Top
Thank you for this post from:
  6/9/2012, 8:05 AM
Joined 5/24/2010
Last visit: 5/1/2013
Posts: 15
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Thanks for reply,

That is what exactly We are looking for,

Can you please leaborate the below as mentioned in the your reply

Send PING command (expansion compared with AG_CNTRL)

Cheeko.
Top
Page 1 of 1 (3 items)
Actions