Technical Forum

OpenModbusTCP

MODBUS TCP LICENSE

Thread Starter: Behrooz   Started: 2/21/2010 2:40 PM   Replies: 5

« Previous thread Next thread »
Page 1 of 1 (6 items)
  2/21/2010, 2:40 PM
Joined 12/1/2007
Last visit: 9/22/2012
Posts: 30
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I want to use modbus tcp, because of that i'm goinig to order: S7- OPEN MODBUS/TCP REDUNDANT FOR S7-400 H SYSTEMS with this order number: 2XV9450-1MB01

is it sufficient to order one package for two cpu or i have to order one package for each CPU?

M.R.Tajalli
Top
  2/21/2010, 5:28 PM
Joined 4/19/2008
Last visit: 5/11/2013
Posts: 1261
Rating:
Rated: Outstanding [3.96 out of 5 / rated 113 time(s)]. (113) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Behrooz wrote:
I want to use modbus tcp, because of that i'm goinig to order: S7- OPEN MODBUS/TCP REDUNDANT FOR S7-400 H SYSTEMS with this order number: 2XV9450-1MB01

is it sufficient to order one package for two cpu or i have to order one package for each CPU?


Hi,

The order No. is Correct, But If you are using with the PCS7 then Please Cheked the Following post & if your CP is Server then Client (Modbus Device) Must be able to polling the both the CP when One CP is Fail, Please Try to Contact Siemens IT People (Germany) for more detail.

Ammy

New for every one..............

“No duty is more urgent than that of returning thanks.”
If Problem Solved......!

Top
  2/22/2010, 8:15 AM
Joined 10/3/2008
Last visit: 5/2/2013
Posts: 522
Rating:
Rated: Outstanding [3.46 out of 5 / rated 52 time(s)]. (52) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,
for 1 h-system (includes 2 CPUs: CPU0 and CPU1) you need 1 license. For a second h-system you would need a second license.

Wüstenräuber
Top
  2/22/2010, 2:57 PM
Joined 12/1/2007
Last visit: 9/22/2012
Posts: 30
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I'm so thankfull.grin

M.R.Tajalli
Top
  5/31/2012, 9:35 AM
Joined 12/7/2011
Last visit: 10/19/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello all,

Just to confirm the earlier pointers.

a.) Assuming I'm using 2 x CPU 417-4H, I will need only one Open Modbus/TCP License.

b.) This Open Modbus/TCP License is required if CPU 400-H is used for interface with 3rd party such as DCS. Please correct me if I misunderstand this.Rnf:lblSmileyTooltip_

Thank you
Murphy
Top
  6/2/2012, 12:50 PM
Joined 11/27/2007
Last visit: 5/25/2013
Posts: 847
Rating:
Rated: Outstanding [3.88 out of 5 / rated 59 time(s)]. (59) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Chan,
yes, you are right.

Regards,
Kaulquappe
Top
Page 1 of 1 (6 items)
Actions