Technical Forum

Communication / Networks

MAS31 - Central Station with Dial Up GSM Modem

Thread Starter: Navnag   Started: 5/26/2012 7:51 PM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  5/26/2012, 7:51 PM
Joined 11/21/2007
Last visit: 5/17/2013
Posts: 539
Rating:
Rated: Excellent [4.04 out of 5 / rated 24 time(s)]. (24) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello

We have an application in which we want to communicate with 8 nos. Remote stations ( With S7-200 + MD720-3 ) .

At the central it is not technically feasible to get a ISP connection with a Static IP. However we are able to install a GSM Modem with STATIC IP Data Activated SIM.

We plan to use a PC with WinCC Flexible + SINAUT Micro-SC  alongwith the connection through the GSM Modem.

Will this configuration work ?

Additionally we need to be able to send / receive SMS to a pre-programmed number from the S7-200 stations while connected to the central station on GPRS. Is this possible ?

Thanks

Navnag

There is no such thing as the last bug in a program
There are no stubborn bugs, There are only stubborn Debuggers.
Top
  5/30/2012, 4:58 PM
Joined 11/21/2007
Last visit: 5/17/2013
Posts: 539
Rating:
Rated: Excellent [4.04 out of 5 / rated 24 time(s)]. (24) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Any suggestions !!

There is no such thing as the last bug in a program
There are no stubborn bugs, There are only stubborn Debuggers.
Top
  5/31/2012, 5:10 PM
Joined 9/29/2005
Last visit: 9/11/2012
Posts: 245
Rating:
Rated: Outstanding [3.94 out of 5 / rated 18 time(s)]. (18) 
Users with special expertise supervising conferences
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Hey,...

wrote:
At the central it is not technically feasible to get a ISP connection with a Static IP. However we are able to install a GSM Modem with STATIC IP Data Activated SIM.

We plan to use a PC with WinCC Flexible + SINAUT Micro-SC  alongwith the connection through the GSM Modem.

Will this configuration work ?


If it is a SIM having a static & public this configuration will work. (Ensure that you will get a REAL public IP address, not a semi-public IP address behind some NAT-mechanism of the provider).

If you have a SIM card with static & private this configuration will work when your SIM cards of your remote station are in the same private network having the permission of your provider to communication with each other. (http://www.marcant.net/ <-- this will work, i have tested it already)

Note that you need to have a modem with port-forwarding functionality. E.g. the Scalance M873-0 will work.


wrote:
Additionally we need to be able to send / receive SMS to a pre-programmed number from the S7-200 stations while connected to the central station on GPRS. Is this possible ?


with the mas31-blocks you cannot switch from opc mode (gprs communication to sinaut micro sc) to at mode (sms communication). in that case you would need a second port (e.ga. cpu 224 xp, or cpu 226) with an separat modem (maybe md720-3) with application mas 5. then your requirements will be possible. i recommand this solution.

if you dont want to have 2x ports and 2xmodems you can use the mas21-blocks where the WDC_CONTROL block is included. you can switch between opc mode and at mode. note that your gprs-connection will be paused during sending sms.

regards
Top
Thank you for this post from:
  7/12/2012, 1:19 PM
Joined 6/4/2012
Last visit: 4/16/2013
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hello,
I wonder why using Scalance M873-0 modem in the control center and not MD720-3 modem, I don't see the difference

Top
Thank you for this post from:
Page 1 of 1 (4 items)
Actions