Technical Forum

Meet & Talk

IEC 61850 application

Thread Starter: taher albiesh   Started: 5/28/2012 10:39 AM   Replies: 7

« Previous thread Next thread »
Page 1 of 1 (8 items)
  5/28/2012, 10:39 AM
Joined 4/3/2012
Last visit: 5/30/2012
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Hi everybody

I’m a student in faculty of mechanical and electrical engineering

I want to achieve the reverse interlocking using goose of IEC 61850.

I have this stuff:

1-      -Protection relays (7sj64) with IEC 61850 module (EN 100).

2-      -PHOENIX switch (FL SWITCH SF8TX).

3-      -DIGSI 4.82.

4-      -KOCOS (FOR TESTING).

The question is:

 Do I need:

1-      -Sicam pas (user interface) to export SCD file.

2-      -IEC 61850 license. (If I need, is there any demo license).

3-      -Industrial switch.

Top
  5/29/2012, 11:57 AM
Joined 11/18/2009
Last visit: 5/7/2013
Posts: 235
Rating:
Rated: Above avarage [3 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
To achive interlocking via IEC 61850 you dont need SICAM PAS.
You can do all this in Digsi and CFC.

Best Regards
Ensar
Top
  5/29/2012, 9:16 PM
Joined 10/9/2007
Last visit: 5/23/2013
Posts: 552
Rating:
Rated: Outstanding [3.62 out of 5 / rated 45 time(s)]. (45) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi


  -Sicam pas (user interface) to export SCD file.
No

2- -IEC 61850 license. (If I need, is there any demo license).
Install Digsi and as License Number enter "Trial". You'll have the full version for 30 days.

3- -Industrial switch.
For such test you don't need special switch. A switch which understands VLAN is enough if you want to see/test the "Goose Priority", which is actually a VLAN priority. Don't connect Siprotec as a ring, as this switch was not tested by Siemens. In digsi configure the EN100 as Line Mode.


Energy Automation products: Sicam, Siprotec, Digsi
Top
  5/30/2012, 12:01 PM
Joined 4/3/2012
Last visit: 5/30/2012
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Thanks a lot Mike j & ensar  for your interest......

I do it successfully via DIGSI only........

But for vertical communication I need IEC 61850 license for sicam pas (UI)

Is there any demo license for sicam pas (UI)???

Top
  5/30/2012, 12:23 PM
Joined 11/18/2009
Last visit: 5/7/2013
Posts: 235
Rating:
Rated: Above avarage [3 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
As far as I can remember when you install SICAM PAS
you can install it like Demo but projects created in Demo
can't be used in licensed version.

Best Regards
Ensar
Top
  5/30/2012, 12:46 PM
Joined 4/3/2012
Last visit: 5/30/2012
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I have sicam pas with UI run time dongle and license but communication between devices via IEC 61850 need another license
except if the demo version come with possibility to communicate devices with each other  via IEC 61850.
Top
  5/30/2012, 1:02 PM
Joined 10/9/2007
Last visit: 5/23/2013
Posts: 552
Rating:
Rated: Outstanding [3.62 out of 5 / rated 45 time(s)]. (45) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hi

yes, the demo version comes with all licenses and works for 3 hours. after that, reboot the computer for more 3 hours.

as Ensar said, a project done in demo version doesn't work on a licensed version.


Mike

Energy Automation products: Sicam, Siprotec, Digsi
Top
  5/30/2012, 1:47 PM
Joined 4/3/2012
Last visit: 5/30/2012
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Thanks for this useful information which will help me so much

Top
Page 1 of 1 (8 items)
Actions