Contact
Home
|
Product Support
|
Applications & Tools
|
Services
|
Forum
|
mySupport
Login
|
Register
Print document
Technical Forum
DC converters SIMOREG
run mill on only single motor by making it master
Thread Starter:
Amit gupta
Started:
5/23/2012 9:44 AM
Replies:
2
« Previous thread
Next thread »
Page 1 of 1 (3 items)
5/23/2012, 9:44 AM
Amit gupta
Joined 5/9/2012
Last visit: 5/25/2012
Posts: 10
Rating:
(0)
(0)
dear experts,
our mill was running on two motors mill master and mill slave,master motor has to remove due to problem in commutator.
now i have to run the mill on only single motor by making it master.i have disconnect the field of slave.now please tell me using the D.C. drive 6ra70. what r the parameters which i must change and after that hw can i run the motor safely.
regards
Amit gupta,
Bhushan steel ltd.
=== Edited by O_Moderator @ 5/23/2012 10:43 AM [GMT ] ===
new subject after splitting from
whole system off during autozeroing on the 6 hi cold rolling mill
Top
5/23/2012, 11:46 AM
KSN
Joined 8/25/2006
Last visit: 6/19/2013
Posts: 909
Rating:
(86)
(0)
Hello.
I think you mean 2 motors that drive top roll and bottom roll of rolling mill, and you have (I think) 2 drives 6RA70. Each 6RA70 controls one motor. Have you any communications between 2 6RA70 or not?
Top
5/25/2012, 10:02 AM
Shank
Joined 9/14/2007
Last visit: 4/9/2013
Posts: 33
Rating:
(2)
(0)
Dear Amit,
Put the parameter of master drive into slave drive. check the peer to peer communication parameter.encoder signal hardwired connected to slave drive.decoupled the common shaft between the two motors.check the current control setpoint which is going from master to slave drive, as well as connect slave drive to field drive via peer to peer communication.
I assume that this two motors are connected with common shaft.
Regards,
Shank
Top
Page 1 of 1 (3 items)
Actions
Copy Link
To conference
Product Conferences
LOGO!
SIMATIC TDC, FM458, T400
SIMATIC S7 - Hardware
SIMATIC S5 / STEP 5
SIMATIC 505
Communication / Networks
Programming Devices
PC-based Automation
Industrial PC SIMATIC PC
Decentral Peripherie
Industrial Software
SIMATIC Addons / IT4Industry
Process Control Systems SIMATIC PCS 7
Teleperm M / WinCC-TM / PCS 7 - TM
Process Control System - APACS+
Process Control System - QUADLOG
Other Process Control Systems
Visualization
SINUMERIK / SIMODRIVES / MASTERDRIVES / SIMOTION / SINAMICS
SINUMERIK CNC automation systems
SIMODRIVE Converter system
SIMOVERT MASTERDRIVES
Motion Control System SIMOTION
SINAMICS
MICROMASTER
ROBICON Perfect Harmony - Medium voltage converters
DC converters SIMOREG
SIMOTICS
Drive Tools
Process Instrumentation / Analytics / Weighing Systems SIWAREX
SIMATIC Ident
Low-Voltage Controls
Building Technology
General Conferences
Quick Links
All Conferences
The new Threads
Highlight Threads
Contact
Support Request
Contacts Worldwide
Moderator
Users online
190B
,
limit
,
Labaz
,
а.м
,
daad
,
NiltonVC26
,
michi33
,
BBPrudente
,
Sridhar_Shunmugavel
,
JNalepka
,
morduna
,
ale_control
,
Tomy Master
,
Hamsterbacke
Help
Online Help
Guided Tour