Technical Forum

SIMODRIVE Converter system

Simple testing digital axis card

Thread Starter: Elektron27   Started: 5/22/2012 9:12 AM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  5/22/2012, 9:12 AM
Joined 6/29/2010
Last visit: 10/8/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
We want to test  a 6SN1118-0DJ23-0AA1 axis card in a basic rack (E/R - NCU572.3  - VSA mod.).
Is it possible to configurate the system only with Sinucom NC or do you always need a PLC program?
We want to do a simple test (jog, forward, reverse).
Can you give a sollwert in Sincom NC?


Thank you and best regards.




=== Edited by Elektron27 @ 5/22/2012 1:24 PM [GMT ] ===


Top
  5/25/2012, 9:12 PM
Joined 12/29/2011
Last visit: 6/7/2012
Posts: 32
Rating:
Rated: Excellent [4.25 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I can't think of an easy solution for you.
SinucomNC is not like SimocomU.
It can't control an axis the way SimocomU
can control and testl a 611U.

You'll need a Machine Control Panel.
Then some s7 plc code to read the signals
from the MCP and code to control the
axis enables and feedback selection.

Plus how are you going to test the
digital axis card will allow messages
to pass through it to control the next
drive card along.?
ie it can work in a drive rack with
3 or 4 other digital drive cards.

Best Regards
Mr_Al
Top
Page 1 of 1 (2 items)
Actions