Technical Forum

SIMOVERT MASTERDRIVES

connect RS232 to master drive X103 port

Thread Starter: putta   Started: 5/21/2012 4:41 AM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  5/21/2012, 4:41 AM
Joined 11/1/2011
Last visit: 3/8/2013
Posts: 58
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
dear sir,

        as per the above instructions to connect RS232 to master drive X103 port, but my Lap Top is does't having the RS232 interface. Then any other solutions regarding? am also faceing same problem please help me how to?



=== Bearbeitet von Blue Moderator @ 21.05.2012 09:48 [GMT ] ===
splitted from 6SE7018-0EP60 master drives AC/AC not communicating via RS232 from PC to x103 and renamed

Top
  5/21/2012, 5:22 AM
Joined 7/8/2009
Last visit: 5/17/2013
Posts: 1167
Rating:
Rated: Excellent [4.25 out of 5 / rated 326 time(s)]. (326) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
For that you need USB to RS232 converter. They are not much reliable but you can read following for help

My PG/PC has only USB com-ports. How I can get online with my drive?


Regards
Devesh Vithani

Please say Thanks if your Problem is Solved.. :-)
Top
  5/21/2012, 1:08 PM
Joined 1/27/2011
Last visit: 9/8/2012
Posts: 38
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 


     Hi,

          I hope it is available anywhere in market.

             The RS232 to USB converter cable Japan make called BAFO cable....

                  U purchase this It ll help U...........

                       U hv to install driver software also......

                           That driver CD also within this cable pack itself



                     
Top
  5/31/2012, 6:14 AM
Joined 11/1/2011
Last visit: 3/8/2013
Posts: 58
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Kutty19 wrote:


     Hi,

          I hope it is available anywhere in market.

             The RS232 to USB converter cable Japan make called BAFO cable....

                  U purchase this It ll help U...........

                       U hv to install driver software also......

                           That driver CD also within this cable pack itself



                     


Dear sir 

  i taken BAFO USB-RS232, and i installed all the drives as given in CD. i am using DrivMon soft, but it is not connected to PC to Master Drive please give me suggition.
Top
  5/31/2012, 7:50 PM
Joined 1/27/2011
Last visit: 9/8/2012
Posts: 38
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 


R u sure your doing proper communication settings in Drive monitor?

Or U change the COM port.

Or U change COM no if more than 10.

Or U try with other PC.

  Thanks.................

 

 

Top
Page 1 of 1 (5 items)
Actions