Technical Forum

Industrial Software general

Meaning of firmware

Erstellt von Chevli am 16.05.2012 13:43 (4 Antworten)

« Vorheriges Thema Nächstes Thema »
Seite 1 von 1 (5 Objekte)
  16.05.2012, 13:43
Beigetreten am: 18.04.2012
Letzter Besuch: 09.07.2012
Beiträge: 34
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Hello Experts,

i am just curious to know about firmware.

Siemens keeps on realeasing new products with updating a firmware every time once it is available to us.


i know about software,hardware but what is this firmware?  
Top
  16.05.2012, 13:48
Beigetreten am: 18.03.2008
Letzter Besuch: 14.05.2013
Beiträge: 1058
Bewertung:
Bewertung: Herausragend [3,96 von 5 / 175 mal bewertet]. (175) 
Hello,

General Defination of firmware:

Firmware is application specific software burned into Hardware.

As far new releases are concern when there are few updates with product it is being delivered by updating a firmware.

Hope this helps.Rnf:lblSmileyTooltip_
Top
  16.05.2012, 15:12
Beigetreten am: 17.01.2007
Letzter Besuch: 17.05.2013
Beiträge: 759
Bewertung:
Bewertung: Exzellent [4,33 von 5 / 141 mal bewertet]. (141) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Hardware is the actual physical devices on the PLC.
Software is the user software than runs on the PLC.
Firmware is the bit in the middle.
Firmware is usually PLC operating system code that is burned into a read only memory of some sort (EPROM, EEPROM etc.). The BIOS of a PC is a good example of firmware. It provides the low level interface between the hardware of the software. Firmware is not routinely changed. It is only updated periodically when implementing bug fixes or adding support for new/changed hardware.

Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots.

So far, the universe is winning...
Top
  17.05.2012, 02:49
Beigetreten am: 13.06.2006
Letzter Besuch: 15.04.2013
Beiträge: 186
Bewertung:
Bewertung: Exzellent [4,83 von 5 / 6 mal bewertet]. (6) 
Bewertung: Exzellent [5 von 5 / 2 mal bewertet]. (2) 
Chevli wrote:
Hello Experts,

i am just curious to know about firmware.

Siemens keeps on realeasing new products with updating a firmware every time once it is available to us.


i know about software,hardware but what is this firmware?  


Hi,
 You only know that the firmware is a special software for the equipments, the firmware is depend on each version of product.
 Every years Siemens update new technology, thus the hardware & firmware has be change too. 
  But sometime we still can use the old firmware for new product. ( eg. Micro master drives ..)


I found this information from internete. This share will helps to more understand.

In electronic systems and computing, firmware is the combination of read-only memory and program code and data stored in it. Typical examples of devices containing firmware are embedded systems, computers, computer peripherals, mobile phones, and digital cameras . The firmware contained in these devices provides the control program for the device. Firmware is held in non-volatile memory devices such as ROM, EPROM, or flash memory. Changing the firmware of a device may rarely or never be done during its economic lifetime; some firmware memory devices are permanently installed and cannot be changed after manufacture. Common reasons for updating firmware include fixing bugs or adding features to the device. This may require physically changing ROM integrated circuits, or reprogramming flash memory with a special procedure. Firmware such as the ROM BIOS of a personal computer may contain only elementary basic functions of a device and may only provide services to higher-level software. Firmware such as the program of an embedded system may be the only program that will run on the system and provide all of its functions.

Regards,
chook


Top
  20.05.2012, 09:22
Beigetreten am: 18.04.2012
Letzter Besuch: 09.07.2012
Beiträge: 34
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Chook wrote:
Chevli wrote:
Hello Experts,

i am just curious to know about firmware.

Siemens keeps on realeasing new products with updating a firmware every time once it is available to us.


i know about software,hardware but what is this firmware?  


Hi,
 You only know that the firmware is a special software for the equipments, the firmware is depend on each version of product.
 Every years Siemens update new technology, thus the hardware & firmware has be change too. 
  But sometime we still can use the old firmware for new product. ( eg. Micro master drives ..)


I found this information from internete. This share will helps to more understand.

In electronic systems and computing, firmware is the combination of read-only memory and program code and data stored in it. Typical examples of devices containing firmware are embedded systems, computers, computer peripherals, mobile phones, and digital cameras . The firmware contained in these devices provides the control program for the device. Firmware is held in non-volatile memory devices such as ROM, EPROM, or flash memory. Changing the firmware of a device may rarely or never be done during its economic lifetime; some firmware memory devices are permanently installed and cannot be changed after manufacture. Common reasons for updating firmware include fixing bugs or adding features to the device. This may require physically changing ROM integrated circuits, or reprogramming flash memory with a special procedure. Firmware such as the ROM BIOS of a personal computer may contain only elementary basic functions of a device and may only provide services to higher-level software. Firmware such as the program of an embedded system may be the only program that will run on the system and provide all of its functions.

Regards,
chook


Thank you chook for detailed answer.
Top
Seite 1 von 1 (5 Objekte)
Aktionen