Technical Forum

MICROMASTER

Induction generator

Thread Starter: Mothilal   Started: 5/18/2012 7:19 AM   Replies: 5

« Previous thread Next thread »
Page 1 of 1 (6 items)
  5/18/2012, 7:19 AM
Joined 11/30/2011
Last visit: 3/12/2013
Posts: 164
Rating:
Rated: Above avarage [3 out of 5 / rated 21 time(s)]. (21) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Dear Experts

   How an Induction motor work as a generator during negative slip condition? This is possible in only slip ring Induction motor?

please let me know..

Thank you

Regards

Mothilal


***ALL IS WELL***
Top
  5/18/2012, 11:19 AM
Joined 7/8/2009
Last visit: 5/21/2013
Posts: 1167
Rating:
Rated: Excellent [4.24 out of 5 / rated 327 time(s)]. (327) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi Mothilal

Yes Any induction motor can work as Indcution Genrator because basic construction for both is same

Motor will be in Generator mode when Load try to Pull the motor. For example, in high inertia load, if you are trying to stop very fast, then load will pull motor so in this case Motor will work as Generator

Best Example is, Hoist application of Crane. During Lowering of hoist, motor will always be in Generative Mode

Regards
Devesh

Please say Thanks if your Problem is Solved.. :-)
Top
Thank you for this post from:
  5/19/2012, 10:04 PM
Joined 3/15/2008
Last visit: 5/25/2013
Posts: 4424
Rating:
Rated: Outstanding [3.88 out of 5 / rated 409 time(s)]. (409) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Mothilal wrote:

Dear Experts

   How an Induction motor work as a generator during negative slip condition? This is possible in only slip ring Induction motor?
...




It is also possible with synchron motor (solenoid rotor)

Industrieautomation: Softwareerstellung und Inbetriebnahme weltweit.
http://www.ibn-service.com
Top
Thank you for this post from:
  5/20/2012, 7:52 AM
Joined 11/30/2011
Last visit: 3/12/2013
Posts: 164
Rating:
Rated: Above avarage [3 out of 5 / rated 21 time(s)]. (21) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hi vithani

   Thanks for ur reply.. Is it possible in squirrel cage induction motor ? Because the induction motor rotor is short circuited.. I have not yet get the clear idea about Induction generator(say ex: wind mill )..If possible please explain me in detail or attach any knowledge bank manual..

Thanks

Regards

Mothilal

***ALL IS WELL***
Top
  5/20/2012, 9:38 AM
Joined 3/15/2008
Last visit: 5/25/2013
Posts: 4424
Rating:
Rated: Outstanding [3.88 out of 5 / rated 409 time(s)]. (409) 
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Ahhhh..

You like to use it as generator only?

Than it is not so very easy.

You must use an induction motor in "island - mode".
(Dont know the correct english word).

But you need a exciter voltage.....

If you like to use a normal induction motor as emergency power generator,
than perhaps it is not a good idea.

Usually the induction motor run as generator if he is connected
to the AC power line that brings exciting voltage to the field.
In this case, he just support the power line as generator but do not
build up the complete voltage by himself only.

Industrieautomation: Softwareerstellung und Inbetriebnahme weltweit.
http://www.ibn-service.com
Top
Thank you for this post from:
  5/20/2012, 5:41 PM
Joined 7/8/2009
Last visit: 5/21/2013
Posts: 1167
Rating:
Rated: Excellent [4.24 out of 5 / rated 327 time(s)]. (327) 
Users with special expertise supervising conferences
Rated: Excellent [5 out of 5 / rated 2 time(s)]. (2) 
I just want to add what IBN has said

You said you have not yet clear idea about Induction Generator then, I think you should start from basics

here is something from google

Induction motor

Induction Generator

How to Use a Three Phase Induction Motor as a Generator

Using Induction Motor as a Generator

OPERATING 60 CYCLE INDUCTION MOTORS AS GENERATORS

Hope this will help you

Regards,
Devesh Vithani



=== Edited by Vithani @ 5/20/2012 5:45 PM [GMT ] ===
Link updated


Please say Thanks if your Problem is Solved.. :-)
Top
Thank you for this post from:
Page 1 of 1 (6 items)
Actions