Technical Forum

Process Control System - QUADLOG

Solution for Programming Quadlog

Thread Starter: MMAB   Started: 4/20/2007 2:47 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  4/20/2007, 2:47 PM
Joined 3/10/2007
Last visit: 6/27/2007
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Think Tanks out there,

I need a PCI slot in my PG, earlier Power PG used to offer this solution, now siemens has closed the powerPG production and sale.

I need PCI slot to connect the MBUS/MNET card for configuring/programming the quadlog using 4-mation.

Any solution?...

Eagerly waiting
Top
  4/23/2007, 5:35 PM
Joined 12/20/2005
Last visit: 4/23/2013
Posts: 78
Rating:
Rated: Excellent [5 out of 5 / rated 3 time(s)]. (3) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello MMAB,

While I am not that familiar with the PG side, if the PG has a standard Ethernet card and the QUADLOG control network has either an APACS Industrial Ethernet Module (IEM) or PC running APACS NIM32 connected to it, then you can use the Ethernet version of 4-mation to make the configuration changes without the need for an additional PCI MBUS Interface card. 
 
Let me know if you have any other questions, otherwise good luck!

RJP
Top
Page 1 of 1 (2 items)
Actions