Dear,
There is no PLC program required for this M19....
But only PLC required for enabling the encoder........
Then U goto setting data parameter 43240 enter some Position or Angel ( 0-359).....
Then U goto MDA run the Spindle in M3/M4 S100 for some time......
Then U give a command M70 M19 or M19 itself......
At this time spindle ll rotate in axes mode and it ll stopped at some angel..
That angel which we had given in that parameter........
While this time the CNC may gives Contour monitoring alarm......
U check the contour deviation value in service display.....
Then U enter the max value in contour tolerence parameter...........
Then it ll be over....................
=== Edited by Kutty19 @ 5/18/2012 7:34 PM [GMT ] ===
|