Good day,
I have been working in the PLC's for quiet some time, but relatively new to drives. My application requires monitoring of 'current, power and actual speed' while only 'speed set point' is being provided to the drive.
Placing the correct 'Connector number's' in the analog output parameters will do the job, but what I couldnt figure out is that how am I supposed to callibrate the output, like for instance, I need
0 V output on 0 KW
and 10 V on 7.5 KW
Precisely, I need to know to use normaliztion parameter in this context.
Secondly, how can I wire up the physical analog input to the actual speed set point and callibrate it accordingly, like 0 V represents 0 RPM and 10 V = 1900 RPM.
Thankyou.