Technical Forum

SIMODRIVE Converter system

Simodrive 611 Power Supply Fault

Thread Starter: Bertus@NBL   Started: 5/8/2012 12:43 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  5/8/2012, 12:43 PM
Joined 5/8/2012
Last visit: 6/19/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi

We have the Following SimoDrive611 system in place for 3x servo motors on a Depalletiser:

SimoDrive 611 (Monitoring) E/R Module Siemens 6SN1145-1BA01-0BA2
SimoDrive 611 (Power) LT Module 2 x 25A Siemens 6SN1123-1AB00-0BA1
SimoDrive 611 (Power) LT Module 1 x 25A Siemens 6SN1123-1AA00-0BA1
SimoDrive 611 Control Unit 2 Axis Siemens 6SN1118-0AE11-0AA1
SimoDrive 611 Control Unit 1 Axis Siemens 6SN1118-0AD11-0AA1


The main supply Fuses for the System blew.

When we replaced the fuses and switch pwer back on.

The green light on Unit 6SN1145-1BA01-0BA2 is On and all other lights of.
The 2x T lights on Unit 6SN1118-0AE11-0AA1 is On.
None of the LED's on Unit 6SN1118-0AD11-0AA1 is On

The Fault on the Machine is Servo Power Supply Fault.

I measure 26 VDC on the DC link Voltage:

Which one of these units are the faulty one?


Top
  5/8/2012, 2:29 PM
Joined 8/4/2009
Last visit: 6/18/2013
Posts: 2348
Rating:
Rated: Excellent [4.12 out of 5 / rated 398 time(s)]. (398) 
Users with special expertise supervising conferences
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 


Hello....

Looks like your enable 63,64,48 is missing...check this....

Any error indication / seven segement display any error is present.

Check it.

Regards,
Prakash

Please no technical questions by Private Message(PM), use the FORUM!!!!!
Top
  5/8/2012, 4:06 PM
Joined 5/8/2012
Last visit: 6/19/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Thanks

I opened up the one power module which had the 2 red LED's lit.

The tracks are burned on the PCB.

So will replace as soon as spare part arrives.

Seems im rusty after the holiday.....

plus I know nothing about these drives.blush
Top
Page 1 of 1 (3 items)
Actions