I have a machine here that I have just upgraded the drive, however I am not too confident on setting up the profibus assignment. I have done some reading about using the GSD file in the drive to get the assignments. The drive is on (Node 5) and the CPU is a 315-2dp s7300 (node 2) with a wincc op (node 9) interface. could anyone assist me in a step by step instruction on how to get the communications up again.
I have entered all the comissioning settings on the starter software like ramp power speed poles etc.. now it is just a matter of getting the data in the correct places.
The old drive used a cb15/cb155 on the midimaster and the g120 has a cu240b-2 DP.. any help is appreciated.
chris
Have u assing Node address in all devices PG/PC settings?
Regard
Deep Bhatt
"The art of being wise is knowing what to overlook"