Hi,
I use the CTRL_HSC -block with: - a pulse on 'CV'
- a DInt-value (=0), from a Datablock, at 'NEW_CV'
- I have put a 1 at 'EN' too (but this shouldn't be necessary)
Is there something I'm missing?
Thank you for your help.
You should not put a pulse on 'CV' of your CTRL_HSC.
You should put the CTRL_HSC in a separate FC or FB.
Then use a pulse to call the FC or FB that includes the CTRL_HSC.
Just call the FC or FB with the parameters that you want to change and always enable the CTRL_HSC in this FC or FB by directly connecting it to left line without any contact.
=== Edited by Gorp @ 5/1/2012 8:31 PM [GMT ] === correction of the text
|
Always read the manuals first.
Then use the "information system" also known as "help".
If that does not bring you further, ask a question but... give all the details!
No need to thank, no need to rate.