Technical Forum

Industrial Software general

step7 installation on Windows7 platform

Thread Starter: Vibha   Started: 4/30/2012 11:02 AM   Replies: 12

« Previous thread Next thread »
12» Page 1 of 2 (13 items)
  4/30/2012, 11:02 AM
Joined 4/19/2011
Last visit: 4/12/2013
Posts: 9
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello everyone.
Simatic Step7 (S7 Prof. V5.4 + SP3.1; S7 SCL V5.3 + SP4) / (Simatic winCC Flexible Adv. 2007) / (Simatic WinCC V7.0 + SP1) can be installed on Windows7 Home Basic + SP1 platform or not. If not, what is the way out? What additional service packs are required? Please suggest.
Top
  4/30/2012, 11:06 AM
Joined 4/30/2008
Last visit: 5/19/2013
Posts: 628
Rating:
Rated: Outstanding [3.94 out of 5 / rated 36 time(s)]. (36) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
https://www.automation.siemens.com/WW/forum/members/PostGetAttachment.aspx?attachmentID=27739&Language=en

Take a look at this

Regards


Steve

Some people are like slinkies
they are really good for nothing
but they still bring a smile to your
face when you push them down the stairs!!!
Top
  4/30/2012, 11:07 AM
Joined 8/25/2006
Last visit: 5/19/2013
Posts: 898
Rating:
Rated: Excellent [4.2 out of 5 / rated 85 time(s)]. (85) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello.
Look here for compatibility.
Top
  4/30/2012, 12:01 PM
Joined 11/18/2010
Last visit: 1/31/2013
Posts: 169
Rating:
Rated: Outstanding [3.13 out of 5 / rated 8 time(s)]. (8) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Vibha wrote:
Hello everyone.
Simatic Step7 (S7 Prof. V5.4 + SP3.1; S7 SCL V5.3 + SP4) / (Simatic winCC Flexible Adv. 2007) / (Simatic WinCC V7.0 + SP1) can be installed on Windows7 Home Basic + SP1 platform or not. If not, what is the way out? What additional service packs are required? Please suggest.




hi ,


you can use s7 manager prof. v5.5
simatic wincc v7.0 sp2 
which are compatible with windows 7

and one good solution you can use VMware for windows xp in windows 7 to run all software as mension by you,

regards,
viral patel
Top
  4/30/2012, 12:08 PM
Joined 5/28/2008
Last visit: 5/19/2013
Posts: 2185
Rating:
Rated: Outstanding [3.65 out of 5 / rated 431 time(s)]. (431) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
To check compatibility between Siemens Program and MS, I like using compatibility tool. till now, it is the latest one (last update 17 Jan. 2012) and I think whenever a new software or SP will be released, it will be updated.
Hope this helps.

Ayman Elotaify
MISC Egypt
www.miscegypt.com
Top
Thank you for this post from:
  4/30/2012, 12:11 PM
Joined 4/30/2012
Last visit: 5/7/2012
Posts: 6
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello vibha
   u just need to install virtual machine in same pc and do whatever u want to install
Top
  4/30/2012, 8:37 PM
Joined 9/27/2005
Last visit: 5/8/2013
Posts: 934
Rating:
Rated: Above avarage [2.61 out of 5 / rated 36 time(s)]. (36) 
as free virtual machine can use XP mode
Top
  4/30/2012, 11:20 PM
Joined 4/20/2007
Last visit: 4/9/2013
Posts: 315
Rating:
Rated: Outstanding [3.61 out of 5 / rated 18 time(s)]. (18) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
bear in mind that Siemens does not support the virtual machines... I have had some problems getting it to work. 

the best solution for me was upgrading to a step 7 that could run on win 7 64 bits
Top
  5/1/2012, 11:18 AM
Joined 9/27/2005
Last visit: 5/8/2013
Posts: 934
Rating:
Rated: Above avarage [2.61 out of 5 / rated 36 time(s)]. (36) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
if you have money, then this is the best blink
Top
  5/1/2012, 11:30 AM
Joined 12/27/2007
Last visit: 5/10/2013
Posts: 251
Rating:
Rated: Very Good [2 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I think VM works well...in certain cases you can download the programme too in the CPU....
VM is a better option if your Computer hardware is good.....if not then you will have to purchase the mentioned software.....

Regards,
Prats
Top
12» Page 1 of 2 (13 items)
Actions