Technical Forum

Meet & Talk

Basic difference between Suggestions -Feedback & Meet & Talk forum

Thread Starter: RAJKIRAN   Started: 4/27/2012 11:23 AM   Replies: 17

« Previous thread Next thread »
12» Page 1 of 2 (18 items)
  4/27/2012, 11:23 AM
Joined 8/18/2009
Last visit: 4/17/2013
Posts: 464
Rating:
Rated: Outstanding [3.63 out of 5 / rated 32 time(s)]. (32) 
Rated: Good [1 out of 5 / rated 2 time(s)]. (2) 
Dear All,
I observe that in both forum(Suggestions -Feedback & Meet & Talk forum), member are given suggetion regarding forum.
now if both is for same platform then why need of two...combine this togther....
also about this post I confuse that which one is right place for published....
may be I am wrong then tell me basic differenc of two conference...
Also tell me this post is in right conference group or not...& why


Rajkiran Patil

Executive Project Eng r.- Process Automation


Top
  4/27/2012, 11:36 AM
Joined 4/30/2008
Last visit: 5/20/2013
Posts: 628
Rating:
Rated: Outstanding [3.94 out of 5 / rated 36 time(s)]. (36) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Suggestions would be for changes or inprovements to the forum
Meet and talk general chat with other members like the weather ,sports score

Regards


Steve

Some people are like slinkies
they are really good for nothing
but they still bring a smile to your
face when you push them down the stairs!!!
Top
  4/27/2012, 11:48 AM
Joined 8/18/2009
Last visit: 4/17/2013
Posts: 464
Rating:
Rated: Outstanding [3.63 out of 5 / rated 32 time(s)]. (32) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
playerslight wrote:
Suggestions would be for changes or inprovements to the forum
Meet and talk general chat with other members like the weather ,sports score

I am not agree that for general chat meet & talk is used.


Rajkiran Patil

Executive Project Eng r.- Process Automation


Top
  4/27/2012, 11:53 AM
Joined 7/8/2009
Last visit: 5/17/2013
Posts: 1167
Rating:
Rated: Excellent [4.25 out of 5 / rated 326 time(s)]. (326) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
playerslight wrote:
Suggestions would be for changes or inprovements to the forum
Meet and talk general chat with other members like the weather ,sports score


For suggestions I am fully AGREE with you. If you have any suggestion or any feedback, you should post it in Suggestions - Feedback conference. If you will post in Meet & talk, Mods will transfer it

For any other discussion - Like any techincal discussion which you cant find any suitable conference, or you have any general question regarding forum or any other thing then you can post them in Meet & Talk Also you can do general chat or congrats any person in Meet & Talk

For Example, feefback and suggestion for campaign is in already in Suggestions - Feedback while this thread is in Meet & Talk 

I hope it is clear now

Regards
Devesh

Please say Thanks if your Problem is Solved.. :-)
Top
Thank you for this post from:
  4/27/2012, 12:01 PM
Joined 11/18/2009
Last visit: 5/7/2013
Posts: 235
Rating:
Rated: Above avarage [3 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Under Meet and Talk members discuse also about problems
for devices/products (mostly Energy Automation Products)
that don't belong to any of the products under Product Conferences.

Mike J is expert on Energy Automation Products
and helps a lot. He helped me when I needed help.
Top
  4/27/2012, 12:06 PM
Joined 8/18/2009
Last visit: 4/17/2013
Posts: 464
Rating:
Rated: Outstanding [3.63 out of 5 / rated 32 time(s)]. (32) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
RAJKIRAN wrote:
Dear All,
Also tell me this post is in right conference group or not...& why

Thanks vithani,
I think your description will be correct, but you are not telling this post is in right place or not...

Rajkiran Patil

Executive Project Eng r.- Process Automation


Top
  4/27/2012, 12:13 PM
Joined 7/8/2009
Last visit: 5/17/2013
Posts: 1167
Rating:
Rated: Excellent [4.25 out of 5 / rated 326 time(s)]. (326) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Vithani wrote:


For Example, feefback and suggestion for campaign is in already in Suggestions - Feedback while this thread is in Meet & Talk 


Dear RAJKIRAN, I already replied that this thread is in Meet & Talk so it is correct

Regards
Devesh

Please say Thanks if your Problem is Solved.. :-)
Top
  4/27/2012, 12:18 PM
Joined 4/8/2011
Last visit: 6/29/2012
Posts: 270
Rating:
Rated: Excellent [4.49 out of 5 / rated 47 time(s)]. (47) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear RAJKIRAN,

to suggest means to make a proposal or to declare a plan for something, feedback is when the information at the end of certain process is sent back to it's start in order to further optimize the whole process and better the results.

On the other hand, to meet means to come together with someone and talking is a process of information exchange between two or more individuals.

As you can see, not every suggestion has to fall in the category of talking, because for that you would first need a feedback from someone else in the respective thread, perhaps someone you've met there.

And even though that doesn't imply the following, it's truth that also not every case of talking with someone you've just met would be a suggestion, because in most cases you are just exchaging opinions for the sake of entertainment, killing time or socializing, not with the direct intention of giving any kind of feedback.

Now that we've met and talk, I suggest you to post your proposals for betterment of the forum in the feedback part.



=== Edited by MM1234 @ 4/27/2012 12:20 PM [GMT ] ===



I don't see why people would still care about travelling salesman problem nowadays. You can simply buy stuff on the internet.
Top
Thank you for this post from:
  4/27/2012, 12:26 PM
Joined 8/18/2009
Last visit: 4/17/2013
Posts: 464
Rating:
Rated: Outstanding [3.63 out of 5 / rated 32 time(s)]. (32) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
RAJKIRAN wrote:
Dear All,
Also tell me this post is in right conference group or not...& why
I think..my above question to other member is may be wrong..because moderator will take decision where is the right place of this post..

Rajkiran Patil

Executive Project Eng r.- Process Automation


Top
  4/27/2012, 12:38 PM
Joined 4/8/2011
Last visit: 6/29/2012
Posts: 270
Rating:
Rated: Excellent [4.49 out of 5 / rated 47 time(s)]. (47) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Of course they eventually will, but you don't have to make them extra work by posting out of the right conference when you can easily distinguish which one is the right one.

I don't see why people would still care about travelling salesman problem nowadays. You can simply buy stuff on the internet.
Top
12» Page 1 of 2 (18 items)
Actions